Hi,
We are trying to have the image of the DA14580 part of the external microcontroller. In your projects you are saving the image in form of an array - "static const char program_t[IMAGE_SIZE] __attribute__((aligned(***))) = {" Is there a tool to convert a .bin file to such an array? How can I produce the array to store in my microcontroller
I am looking for a tool to convert the Intel Hex file into a array, as the array can be used for serial bootloading. As shown in the SDK 5.0.4 example code
SDK 5.0.4\DA1458x_SDK_5.0.4\DA1458x_SDK\5.0.4\projects\host_apps\da1458x\proximity\reporter\include\prox_reporter_ext.h file.