こんにちは。NoMaYです。今、以下のスレッドに投稿しているのですけれども、派生ネタが思い浮かびましたので、またひとつ立ててみました。RXv3コアのレジスタ一括退避機能の使い方(Register Bank Save Function Usage)を調べてみるスレッドcommunity-ja.renesas.com/cafe_rene/forums-groups/mcu-mpu/rx/f/forum5/9572/rxv3-register-bank-save-function-usage派生ネタ・ 以下のスレッドのやり方にてライブラリを作る・ 単にSETPSW Iする方式ではなく、IPLを操作した後にSETPSW Iする方式とする・ RXv3コアだけでなく、RXv1コアやRXv2コアでも動作するようにする・ 実用になるかどうかは未知数ですスレッドスマートコンフィグレータの自動生成をカスタマイズしたいcommunity-ja.renesas.com/cafe_rene/forums-groups/mcu-mpu/rx/f/forum5/8248/thread/42690#42690MISPOさんのNORTiをRX SmartConfiguratorと一緒に使いたい場合の課題と対策を考察してみるスレッドcommunity-ja.renesas.com/cafe_rene/forums-groups/tools/f/forum21/8266/mispo-norti-rx-smartconfigurator/42873#42873
こんにちは。NoMaYです。まず、CC-RX版をひとつ作ってみました。以下、肝心な部分のソースとe2 studioでシミュレータデバッグ中の画面コピーです。(肝心な部分は他にはありません。)NestedIntLib.c
/* * NestedIntLib.c * * Created on: Dec 06, 2022 * Author: NoMaY * License: MIT */ #include "r_smc_entry.h" #include "NestedIntLib.h" static void (* const Int_Hook_Vectors[])(void); void NESTEDINTLIB_INT_HOOK_init(void) { set_intb((void *)Int_Hook_Vectors); } static void dummy_NESTEDINTLIB_INT_HOOK_init(void) { // To prevent developers from being misled regarding the following inline assemble errors. // E0552111:Symbol is undefined // E0552113:Symbol definition is not appropriate // E0552052:Addressing mode specifier is not appropriate // or various inline assemble errors for(;;); } // Convert `0xX` format --> `DD` format for CC-RX inline assembler. #if BSP_CFG_FIT_IPL_MAX >= 16 #error "BSP_CFG_FIT_IPL_MAX should be 0x0 - 0xF." #elif BSP_CFG_FIT_IPL_MAX == 15 #define _BSP_CFG_FIT_IPL_MAX 15 #elif BSP_CFG_FIT_IPL_MAX == 14 #define _BSP_CFG_FIT_IPL_MAX 14 #elif BSP_CFG_FIT_IPL_MAX == 13 #define _BSP_CFG_FIT_IPL_MAX 13 #elif BSP_CFG_FIT_IPL_MAX == 12 #define _BSP_CFG_FIT_IPL_MAX 12 #elif BSP_CFG_FIT_IPL_MAX == 11 #define _BSP_CFG_FIT_IPL_MAX 11 #elif BSP_CFG_FIT_IPL_MAX == 10 #define _BSP_CFG_FIT_IPL_MAX 10 #elif BSP_CFG_FIT_IPL_MAX == 9 #define _BSP_CFG_FIT_IPL_MAX 9 #elif BSP_CFG_FIT_IPL_MAX == 8 #define _BSP_CFG_FIT_IPL_MAX 8 #elif BSP_CFG_FIT_IPL_MAX == 7 #define _BSP_CFG_FIT_IPL_MAX 7 #elif BSP_CFG_FIT_IPL_MAX == 6 #define _BSP_CFG_FIT_IPL_MAX 6 #elif BSP_CFG_FIT_IPL_MAX == 5 #define _BSP_CFG_FIT_IPL_MAX 5 #elif BSP_CFG_FIT_IPL_MAX == 4 #define _BSP_CFG_FIT_IPL_MAX 4 #elif BSP_CFG_FIT_IPL_MAX == 3 #define _BSP_CFG_FIT_IPL_MAX 3 #elif BSP_CFG_FIT_IPL_MAX == 2 #define _BSP_CFG_FIT_IPL_MAX 2 #elif BSP_CFG_FIT_IPL_MAX == 1 #define _BSP_CFG_FIT_IPL_MAX 1 #elif BSP_CFG_FIT_IPL_MAX == 0 #define _BSP_CFG_FIT_IPL_MAX 0 #else #error "BSP_CFG_FIT_IPL_MAX should be 0x0 - 0xF." #endif #pragma inline_asm INT_COMMON_NESTEDINT_PERMIT static void INT_COMMON_NESTEDINT_PERMIT(void) { PUSH.L R15 MVFC PSW, R15 #ifdef __RXV3 BFMOVZ #24, #0, #4, R15, R15 #else SHLR #24, R5 AND #15, R5 #endif CMP #_BSP_CFG_FIT_IPL_MAX, R15 BGEU ?+ MVTIPL #_BSP_CFG_FIT_IPL_MAX ?: SETPSW I MOV.L 4[SP], R15 // address of hook_entry_XXX + 3 --> R15 ADD #(- (__$hook_entry___0 + 3) + TOPOF C$VECT), R15 // 3 = size of BSR.W MOV.L [R15], 4[SP] RTSD #4, R15-R15 // i.e. POP R15, JMP [SP+] } #pragma inline_asm INT_COMMON_NESTEDINT_NOT_PERMIT static void INT_COMMON_NESTEDINT_NOT_PERMIT(void) { XCHG [SP], R15 // address of hook_entry_XXX + 3 --> R15 ADD #(- (__$hook_entry___0 + 3) + TOPOF C$VECT), R15 // 3 = size of BSR.W MOV.L [R15], R15 XCHG [SP], R15 RTS // i.e. JMP [SP+] } #pragma inline_asm INT_ENTRY_NESTEDINT_PERMIT static void INT_ENTRY_NESTEDINT_PERMIT(void) { BSR.W __$INT_COMMON_NESTEDINT_PERMIT } #pragma inline_asm INT_ENTRY_NESTEDINT_NOT_PERMIT static void INT_ENTRY_NESTEDINT_NOT_PERMIT(void) { BSR.W __$INT_COMMON_NESTEDINT_NOT_PERMIT } // Documents // https://www.renesas.com/us/en/document/mas/rx-family-rxv1-instruction-set-architecture-users-manual-software-rev130 // https://www.renesas.com/jp/ja/document/mas/rx-family-rxv2-instruction-set-architecture-users-manual-software // https://www.renesas.com/jp/ja/document/mas/rx-family-rxv3-instruction-set-architecture-users-manual-software-rev100 // To prevent the symbol from being optimized out. void * const dummy_INT_COMMON_NESTEDINT_NOT_PERMIT = (void *)INT_COMMON_NESTEDINT_NOT_PERMIT; void * const dummy_INT_COMMON_NESTEDINT_PERMIT = (void *)INT_COMMON_NESTEDINT_PERMIT; // To prevent the section name symbol `C$VECT` from being optimized out. void * const dummy_VECTTBL = (void *)__sectop("C$VECT"); // To prevent a compile warning. void * const dummy2_NESTEDINTLIB_INT_HOOK_init = (void *)dummy_NESTEDINTLIB_INT_HOOK_init; // The code size of the following functions is just 4 bytes. // For NOT_PERMIT // 00000000 39rrrr W BSR.W __$INT_COMMON_NESTEDINT_NOT_PERMIT // 00000003 02 RTS // Not used. // For PERMIT // 00000000 39rrrr W BSR.W __$INT_COMMON_NESTEDINT_PERMIT // 00000003 02 RTS // Not used. #define _INT_ENTRY(sel) INT_ENTRY_NESTEDINT_##sel() #define INT_ENTRY(sel) _INT_ENTRY(sel) static void hook_entry___0(void) { INT_ENTRY(INTERRUPT___0); } static void hook_entry___1(void) { INT_ENTRY(INTERRUPT___1); } static void hook_entry___2(void) { INT_ENTRY(INTERRUPT___2); } static void hook_entry___3(void) { INT_ENTRY(INTERRUPT___3); } static void hook_entry___4(void) { INT_ENTRY(INTERRUPT___4); } static void hook_entry___5(void) { INT_ENTRY(INTERRUPT___5); } static void hook_entry___6(void) { INT_ENTRY(INTERRUPT___6); } static void hook_entry___7(void) { INT_ENTRY(INTERRUPT___7); } static void hook_entry___8(void) { INT_ENTRY(INTERRUPT___8); } static void hook_entry___9(void) { INT_ENTRY(INTERRUPT___9); } static void hook_entry__10(void) { INT_ENTRY(INTERRUPT__10); } static void hook_entry__11(void) { INT_ENTRY(INTERRUPT__11); } static void hook_entry__12(void) { INT_ENTRY(INTERRUPT__12); } static void hook_entry__13(void) { INT_ENTRY(INTERRUPT__13); } static void hook_entry__14(void) { INT_ENTRY(INTERRUPT__14); } static void hook_entry__15(void) { INT_ENTRY(INTERRUPT__15); } static void hook_entry__16(void) { INT_ENTRY(INTERRUPT__16); } static void hook_entry__17(void) { INT_ENTRY(INTERRUPT__17); } static void hook_entry__18(void) { INT_ENTRY(INTERRUPT__18); } static void hook_entry__19(void) { INT_ENTRY(INTERRUPT__19); } static void hook_entry__20(void) { INT_ENTRY(INTERRUPT__20); } static void hook_entry__21(void) { INT_ENTRY(INTERRUPT__21); } static void hook_entry__22(void) { INT_ENTRY(INTERRUPT__22); } static void hook_entry__23(void) { INT_ENTRY(INTERRUPT__23); } static void hook_entry__24(void) { INT_ENTRY(INTERRUPT__24); } static void hook_entry__25(void) { INT_ENTRY(INTERRUPT__25); } static void hook_entry__26(void) { INT_ENTRY(INTERRUPT__26); } static void hook_entry__27(void) { INT_ENTRY(INTERRUPT__27); } static void hook_entry__28(void) { INT_ENTRY(INTERRUPT__28); } static void hook_entry__29(void) { INT_ENTRY(INTERRUPT__29); } static void hook_entry__30(void) { INT_ENTRY(INTERRUPT__30); } static void hook_entry__31(void) { INT_ENTRY(INTERRUPT__31); } static void hook_entry__32(void) { INT_ENTRY(INTERRUPT__32); } static void hook_entry__33(void) { INT_ENTRY(INTERRUPT__33); } static void hook_entry__34(void) { INT_ENTRY(INTERRUPT__34); } static void hook_entry__35(void) { INT_ENTRY(INTERRUPT__35); } static void hook_entry__36(void) { INT_ENTRY(INTERRUPT__36); } static void hook_entry__37(void) { INT_ENTRY(INTERRUPT__37); } static void hook_entry__38(void) { INT_ENTRY(INTERRUPT__38); } static void hook_entry__39(void) { INT_ENTRY(INTERRUPT__39); } static void hook_entry__40(void) { INT_ENTRY(INTERRUPT__40); } static void hook_entry__41(void) { INT_ENTRY(INTERRUPT__41); } static void hook_entry__42(void) { INT_ENTRY(INTERRUPT__42); } static void hook_entry__43(void) { INT_ENTRY(INTERRUPT__43); } static void hook_entry__44(void) { INT_ENTRY(INTERRUPT__44); } static void hook_entry__45(void) { INT_ENTRY(INTERRUPT__45); } static void hook_entry__46(void) { INT_ENTRY(INTERRUPT__46); } static void hook_entry__47(void) { INT_ENTRY(INTERRUPT__47); } static void hook_entry__48(void) { INT_ENTRY(INTERRUPT__48); } static void hook_entry__49(void) { INT_ENTRY(INTERRUPT__49); } static void hook_entry__50(void) { INT_ENTRY(INTERRUPT__50); } static void hook_entry__51(void) { INT_ENTRY(INTERRUPT__51); } static void hook_entry__52(void) { INT_ENTRY(INTERRUPT__52); } static void hook_entry__53(void) { INT_ENTRY(INTERRUPT__53); } static void hook_entry__54(void) { INT_ENTRY(INTERRUPT__54); } static void hook_entry__55(void) { INT_ENTRY(INTERRUPT__55); } static void hook_entry__56(void) { INT_ENTRY(INTERRUPT__56); } static void hook_entry__57(void) { INT_ENTRY(INTERRUPT__57); } static void hook_entry__58(void) { INT_ENTRY(INTERRUPT__58); } static void hook_entry__59(void) { INT_ENTRY(INTERRUPT__59); } static void hook_entry__60(void) { INT_ENTRY(INTERRUPT__60); } static void hook_entry__61(void) { INT_ENTRY(INTERRUPT__61); } static void hook_entry__62(void) { INT_ENTRY(INTERRUPT__62); } static void hook_entry__63(void) { INT_ENTRY(INTERRUPT__63); } static void hook_entry__64(void) { INT_ENTRY(INTERRUPT__64); } static void hook_entry__65(void) { INT_ENTRY(INTERRUPT__65); } static void hook_entry__66(void) { INT_ENTRY(INTERRUPT__66); } static void hook_entry__67(void) { INT_ENTRY(INTERRUPT__67); } static void hook_entry__68(void) { INT_ENTRY(INTERRUPT__68); } static void hook_entry__69(void) { INT_ENTRY(INTERRUPT__69); } static void hook_entry__70(void) { INT_ENTRY(INTERRUPT__70); } static void hook_entry__71(void) { INT_ENTRY(INTERRUPT__71); } static void hook_entry__72(void) { INT_ENTRY(INTERRUPT__72); } static void hook_entry__73(void) { INT_ENTRY(INTERRUPT__73); } static void hook_entry__74(void) { INT_ENTRY(INTERRUPT__74); } static void hook_entry__75(void) { INT_ENTRY(INTERRUPT__75); } static void hook_entry__76(void) { INT_ENTRY(INTERRUPT__76); } static void hook_entry__77(void) { INT_ENTRY(INTERRUPT__77); } static void hook_entry__78(void) { INT_ENTRY(INTERRUPT__78); } static void hook_entry__79(void) { INT_ENTRY(INTERRUPT__79); } static void hook_entry__80(void) { INT_ENTRY(INTERRUPT__80); } static void hook_entry__81(void) { INT_ENTRY(INTERRUPT__81); } static void hook_entry__82(void) { INT_ENTRY(INTERRUPT__82); } static void hook_entry__83(void) { INT_ENTRY(INTERRUPT__83); } static void hook_entry__84(void) { INT_ENTRY(INTERRUPT__84); } static void hook_entry__85(void) { INT_ENTRY(INTERRUPT__85); } static void hook_entry__86(void) { INT_ENTRY(INTERRUPT__86); } static void hook_entry__87(void) { INT_ENTRY(INTERRUPT__87); } static void hook_entry__88(void) { INT_ENTRY(INTERRUPT__88); } static void hook_entry__89(void) { INT_ENTRY(INTERRUPT__89); } static void hook_entry__90(void) { INT_ENTRY(INTERRUPT__90); } static void hook_entry__91(void) { INT_ENTRY(INTERRUPT__91); } static void hook_entry__92(void) { INT_ENTRY(INTERRUPT__92); } static void hook_entry__93(void) { INT_ENTRY(INTERRUPT__93); } static void hook_entry__94(void) { INT_ENTRY(INTERRUPT__94); } static void hook_entry__95(void) { INT_ENTRY(INTERRUPT__95); } static void hook_entry__96(void) { INT_ENTRY(INTERRUPT__96); } static void hook_entry__97(void) { INT_ENTRY(INTERRUPT__97); } static void hook_entry__98(void) { INT_ENTRY(INTERRUPT__98); } static void hook_entry__99(void) { INT_ENTRY(INTERRUPT__99); } static void hook_entry_100(void) { INT_ENTRY(INTERRUPT_100); } static void hook_entry_101(void) { INT_ENTRY(INTERRUPT_101); } static void hook_entry_102(void) { INT_ENTRY(INTERRUPT_102); } static void hook_entry_103(void) { INT_ENTRY(INTERRUPT_103); } static void hook_entry_104(void) { INT_ENTRY(INTERRUPT_104); } static void hook_entry_105(void) { INT_ENTRY(INTERRUPT_105); } static void hook_entry_106(void) { INT_ENTRY(INTERRUPT_106); } static void hook_entry_107(void) { INT_ENTRY(INTERRUPT_107); } static void hook_entry_108(void) { INT_ENTRY(INTERRUPT_108); } static void hook_entry_109(void) { INT_ENTRY(INTERRUPT_109); } static void hook_entry_110(void) { INT_ENTRY(INTERRUPT_110); } static void hook_entry_111(void) { INT_ENTRY(INTERRUPT_111); } static void hook_entry_112(void) { INT_ENTRY(INTERRUPT_112); } static void hook_entry_113(void) { INT_ENTRY(INTERRUPT_113); } static void hook_entry_114(void) { INT_ENTRY(INTERRUPT_114); } static void hook_entry_115(void) { INT_ENTRY(INTERRUPT_115); } static void hook_entry_116(void) { INT_ENTRY(INTERRUPT_116); } static void hook_entry_117(void) { INT_ENTRY(INTERRUPT_117); } static void hook_entry_118(void) { INT_ENTRY(INTERRUPT_118); } static void hook_entry_119(void) { INT_ENTRY(INTERRUPT_119); } static void hook_entry_120(void) { INT_ENTRY(INTERRUPT_120); } static void hook_entry_121(void) { INT_ENTRY(INTERRUPT_121); } static void hook_entry_122(void) { INT_ENTRY(INTERRUPT_122); } static void hook_entry_123(void) { INT_ENTRY(INTERRUPT_123); } static void hook_entry_124(void) { INT_ENTRY(INTERRUPT_124); } static void hook_entry_125(void) { INT_ENTRY(INTERRUPT_125); } static void hook_entry_126(void) { INT_ENTRY(INTERRUPT_126); } static void hook_entry_127(void) { INT_ENTRY(INTERRUPT_127); } static void hook_entry_128(void) { INT_ENTRY(INTERRUPT_128); } static void hook_entry_129(void) { INT_ENTRY(INTERRUPT_129); } static void hook_entry_130(void) { INT_ENTRY(INTERRUPT_130); } static void hook_entry_131(void) { INT_ENTRY(INTERRUPT_131); } static void hook_entry_132(void) { INT_ENTRY(INTERRUPT_132); } static void hook_entry_133(void) { INT_ENTRY(INTERRUPT_133); } static void hook_entry_134(void) { INT_ENTRY(INTERRUPT_134); } static void hook_entry_135(void) { INT_ENTRY(INTERRUPT_135); } static void hook_entry_136(void) { INT_ENTRY(INTERRUPT_136); } static void hook_entry_137(void) { INT_ENTRY(INTERRUPT_137); } static void hook_entry_138(void) { INT_ENTRY(INTERRUPT_138); } static void hook_entry_139(void) { INT_ENTRY(INTERRUPT_139); } static void hook_entry_140(void) { INT_ENTRY(INTERRUPT_140); } static void hook_entry_141(void) { INT_ENTRY(INTERRUPT_141); } static void hook_entry_142(void) { INT_ENTRY(INTERRUPT_142); } static void hook_entry_143(void) { INT_ENTRY(INTERRUPT_143); } static void hook_entry_144(void) { INT_ENTRY(INTERRUPT_144); } static void hook_entry_145(void) { INT_ENTRY(INTERRUPT_145); } static void hook_entry_146(void) { INT_ENTRY(INTERRUPT_146); } static void hook_entry_147(void) { INT_ENTRY(INTERRUPT_147); } static void hook_entry_148(void) { INT_ENTRY(INTERRUPT_148); } static void hook_entry_149(void) { INT_ENTRY(INTERRUPT_149); } static void hook_entry_150(void) { INT_ENTRY(INTERRUPT_150); } static void hook_entry_151(void) { INT_ENTRY(INTERRUPT_151); } static void hook_entry_152(void) { INT_ENTRY(INTERRUPT_152); } static void hook_entry_153(void) { INT_ENTRY(INTERRUPT_153); } static void hook_entry_154(void) { INT_ENTRY(INTERRUPT_154); } static void hook_entry_155(void) { INT_ENTRY(INTERRUPT_155); } static void hook_entry_156(void) { INT_ENTRY(INTERRUPT_156); } static void hook_entry_157(void) { INT_ENTRY(INTERRUPT_157); } static void hook_entry_158(void) { INT_ENTRY(INTERRUPT_158); } static void hook_entry_159(void) { INT_ENTRY(INTERRUPT_159); } static void hook_entry_160(void) { INT_ENTRY(INTERRUPT_160); } static void hook_entry_161(void) { INT_ENTRY(INTERRUPT_161); } static void hook_entry_162(void) { INT_ENTRY(INTERRUPT_162); } static void hook_entry_163(void) { INT_ENTRY(INTERRUPT_163); } static void hook_entry_164(void) { INT_ENTRY(INTERRUPT_164); } static void hook_entry_165(void) { INT_ENTRY(INTERRUPT_165); } static void hook_entry_166(void) { INT_ENTRY(INTERRUPT_166); } static void hook_entry_167(void) { INT_ENTRY(INTERRUPT_167); } static void hook_entry_168(void) { INT_ENTRY(INTERRUPT_168); } static void hook_entry_169(void) { INT_ENTRY(INTERRUPT_169); } static void hook_entry_170(void) { INT_ENTRY(INTERRUPT_170); } static void hook_entry_171(void) { INT_ENTRY(INTERRUPT_171); } static void hook_entry_172(void) { INT_ENTRY(INTERRUPT_172); } static void hook_entry_173(void) { INT_ENTRY(INTERRUPT_173); } static void hook_entry_174(void) { INT_ENTRY(INTERRUPT_174); } static void hook_entry_175(void) { INT_ENTRY(INTERRUPT_175); } static void hook_entry_176(void) { INT_ENTRY(INTERRUPT_176); } static void hook_entry_177(void) { INT_ENTRY(INTERRUPT_177); } static void hook_entry_178(void) { INT_ENTRY(INTERRUPT_178); } static void hook_entry_179(void) { INT_ENTRY(INTERRUPT_179); } static void hook_entry_180(void) { INT_ENTRY(INTERRUPT_180); } static void hook_entry_181(void) { INT_ENTRY(INTERRUPT_181); } static void hook_entry_182(void) { INT_ENTRY(INTERRUPT_182); } static void hook_entry_183(void) { INT_ENTRY(INTERRUPT_183); } static void hook_entry_184(void) { INT_ENTRY(INTERRUPT_184); } static void hook_entry_185(void) { INT_ENTRY(INTERRUPT_185); } static void hook_entry_186(void) { INT_ENTRY(INTERRUPT_186); } static void hook_entry_187(void) { INT_ENTRY(INTERRUPT_187); } static void hook_entry_188(void) { INT_ENTRY(INTERRUPT_188); } static void hook_entry_189(void) { INT_ENTRY(INTERRUPT_189); } static void hook_entry_190(void) { INT_ENTRY(INTERRUPT_190); } static void hook_entry_191(void) { INT_ENTRY(INTERRUPT_191); } static void hook_entry_192(void) { INT_ENTRY(INTERRUPT_192); } static void hook_entry_193(void) { INT_ENTRY(INTERRUPT_193); } static void hook_entry_194(void) { INT_ENTRY(INTERRUPT_194); } static void hook_entry_195(void) { INT_ENTRY(INTERRUPT_195); } static void hook_entry_196(void) { INT_ENTRY(INTERRUPT_196); } static void hook_entry_197(void) { INT_ENTRY(INTERRUPT_197); } static void hook_entry_198(void) { INT_ENTRY(INTERRUPT_198); } static void hook_entry_199(void) { INT_ENTRY(INTERRUPT_199); } static void hook_entry_200(void) { INT_ENTRY(INTERRUPT_200); } static void hook_entry_201(void) { INT_ENTRY(INTERRUPT_201); } static void hook_entry_202(void) { INT_ENTRY(INTERRUPT_202); } static void hook_entry_203(void) { INT_ENTRY(INTERRUPT_203); } static void hook_entry_204(void) { INT_ENTRY(INTERRUPT_204); } static void hook_entry_205(void) { INT_ENTRY(INTERRUPT_205); } static void hook_entry_206(void) { INT_ENTRY(INTERRUPT_206); } static void hook_entry_207(void) { INT_ENTRY(INTERRUPT_207); } static void hook_entry_208(void) { INT_ENTRY(INTERRUPT_208); } static void hook_entry_209(void) { INT_ENTRY(INTERRUPT_209); } static void hook_entry_210(void) { INT_ENTRY(INTERRUPT_210); } static void hook_entry_211(void) { INT_ENTRY(INTERRUPT_211); } static void hook_entry_212(void) { INT_ENTRY(INTERRUPT_212); } static void hook_entry_213(void) { INT_ENTRY(INTERRUPT_213); } static void hook_entry_214(void) { INT_ENTRY(INTERRUPT_214); } static void hook_entry_215(void) { INT_ENTRY(INTERRUPT_215); } static void hook_entry_216(void) { INT_ENTRY(INTERRUPT_216); } static void hook_entry_217(void) { INT_ENTRY(INTERRUPT_217); } static void hook_entry_218(void) { INT_ENTRY(INTERRUPT_218); } static void hook_entry_219(void) { INT_ENTRY(INTERRUPT_219); } static void hook_entry_220(void) { INT_ENTRY(INTERRUPT_220); } static void hook_entry_221(void) { INT_ENTRY(INTERRUPT_221); } static void hook_entry_222(void) { INT_ENTRY(INTERRUPT_222); } static void hook_entry_223(void) { INT_ENTRY(INTERRUPT_223); } static void hook_entry_224(void) { INT_ENTRY(INTERRUPT_224); } static void hook_entry_225(void) { INT_ENTRY(INTERRUPT_225); } static void hook_entry_226(void) { INT_ENTRY(INTERRUPT_226); } static void hook_entry_227(void) { INT_ENTRY(INTERRUPT_227); } static void hook_entry_228(void) { INT_ENTRY(INTERRUPT_228); } static void hook_entry_229(void) { INT_ENTRY(INTERRUPT_229); } static void hook_entry_230(void) { INT_ENTRY(INTERRUPT_230); } static void hook_entry_231(void) { INT_ENTRY(INTERRUPT_231); } static void hook_entry_232(void) { INT_ENTRY(INTERRUPT_232); } static void hook_entry_233(void) { INT_ENTRY(INTERRUPT_233); } static void hook_entry_234(void) { INT_ENTRY(INTERRUPT_234); } static void hook_entry_235(void) { INT_ENTRY(INTERRUPT_235); } static void hook_entry_236(void) { INT_ENTRY(INTERRUPT_236); } static void hook_entry_237(void) { INT_ENTRY(INTERRUPT_237); } static void hook_entry_238(void) { INT_ENTRY(INTERRUPT_238); } static void hook_entry_239(void) { INT_ENTRY(INTERRUPT_239); } static void hook_entry_240(void) { INT_ENTRY(INTERRUPT_240); } static void hook_entry_241(void) { INT_ENTRY(INTERRUPT_241); } static void hook_entry_242(void) { INT_ENTRY(INTERRUPT_242); } static void hook_entry_243(void) { INT_ENTRY(INTERRUPT_243); } static void hook_entry_244(void) { INT_ENTRY(INTERRUPT_244); } static void hook_entry_245(void) { INT_ENTRY(INTERRUPT_245); } static void hook_entry_246(void) { INT_ENTRY(INTERRUPT_246); } static void hook_entry_247(void) { INT_ENTRY(INTERRUPT_247); } static void hook_entry_248(void) { INT_ENTRY(INTERRUPT_248); } static void hook_entry_249(void) { INT_ENTRY(INTERRUPT_249); } static void hook_entry_250(void) { INT_ENTRY(INTERRUPT_250); } static void hook_entry_251(void) { INT_ENTRY(INTERRUPT_251); } static void hook_entry_252(void) { INT_ENTRY(INTERRUPT_252); } static void hook_entry_253(void) { INT_ENTRY(INTERRUPT_253); } static void hook_entry_254(void) { INT_ENTRY(INTERRUPT_254); } static void hook_entry_255(void) { INT_ENTRY(INTERRUPT_255); } static void (* const Int_Hook_Vectors[])(void) = { (void (*)(void))hook_entry___0, (void (*)(void))hook_entry___1, (void (*)(void))hook_entry___2, (void (*)(void))hook_entry___3, (void (*)(void))hook_entry___4, (void (*)(void))hook_entry___5, (void (*)(void))hook_entry___6, (void (*)(void))hook_entry___7, (void (*)(void))hook_entry___8, (void (*)(void))hook_entry___9, (void (*)(void))hook_entry__10, (void (*)(void))hook_entry__11, (void (*)(void))hook_entry__12, (void (*)(void))hook_entry__13, (void (*)(void))hook_entry__14, (void (*)(void))hook_entry__15, (void (*)(void))hook_entry__16, (void (*)(void))hook_entry__17, (void (*)(void))hook_entry__18, (void (*)(void))hook_entry__19, (void (*)(void))hook_entry__20, (void (*)(void))hook_entry__21, (void (*)(void))hook_entry__22, (void (*)(void))hook_entry__23, (void (*)(void))hook_entry__24, (void (*)(void))hook_entry__25, (void (*)(void))hook_entry__26, (void (*)(void))hook_entry__27, (void (*)(void))hook_entry__28, (void (*)(void))hook_entry__29, (void (*)(void))hook_entry__30, (void (*)(void))hook_entry__31, (void (*)(void))hook_entry__32, (void (*)(void))hook_entry__33, (void (*)(void))hook_entry__34, (void (*)(void))hook_entry__35, (void (*)(void))hook_entry__36, (void (*)(void))hook_entry__37, (void (*)(void))hook_entry__38, (void (*)(void))hook_entry__39, (void (*)(void))hook_entry__40, (void (*)(void))hook_entry__41, (void (*)(void))hook_entry__42, (void (*)(void))hook_entry__43, (void (*)(void))hook_entry__44, (void (*)(void))hook_entry__45, (void (*)(void))hook_entry__46, (void (*)(void))hook_entry__47, (void (*)(void))hook_entry__48, (void (*)(void))hook_entry__49, (void (*)(void))hook_entry__50, (void (*)(void))hook_entry__51, (void (*)(void))hook_entry__52, (void (*)(void))hook_entry__53, (void (*)(void))hook_entry__54, (void (*)(void))hook_entry__55, (void (*)(void))hook_entry__56, (void (*)(void))hook_entry__57, (void (*)(void))hook_entry__58, (void (*)(void))hook_entry__59, (void (*)(void))hook_entry__60, (void (*)(void))hook_entry__61, (void (*)(void))hook_entry__62, (void (*)(void))hook_entry__63, (void (*)(void))hook_entry__64, (void (*)(void))hook_entry__65, (void (*)(void))hook_entry__66, (void (*)(void))hook_entry__67, (void (*)(void))hook_entry__68, (void (*)(void))hook_entry__69, (void (*)(void))hook_entry__70, (void (*)(void))hook_entry__71, (void (*)(void))hook_entry__72, (void (*)(void))hook_entry__73, (void (*)(void))hook_entry__74, (void (*)(void))hook_entry__75, (void (*)(void))hook_entry__76, (void (*)(void))hook_entry__77, (void (*)(void))hook_entry__78, (void (*)(void))hook_entry__79, (void (*)(void))hook_entry__80, (void (*)(void))hook_entry__81, (void (*)(void))hook_entry__82, (void (*)(void))hook_entry__83, (void (*)(void))hook_entry__84, (void (*)(void))hook_entry__85, (void (*)(void))hook_entry__86, (void (*)(void))hook_entry__87, (void (*)(void))hook_entry__88, (void (*)(void))hook_entry__89, (void (*)(void))hook_entry__90, (void (*)(void))hook_entry__91, (void (*)(void))hook_entry__92, (void (*)(void))hook_entry__93, (void (*)(void))hook_entry__94, (void (*)(void))hook_entry__95, (void (*)(void))hook_entry__96, (void (*)(void))hook_entry__97, (void (*)(void))hook_entry__98, (void (*)(void))hook_entry__99, (void (*)(void))hook_entry_100, (void (*)(void))hook_entry_101, (void (*)(void))hook_entry_102, (void (*)(void))hook_entry_103, (void (*)(void))hook_entry_104, (void (*)(void))hook_entry_105, (void (*)(void))hook_entry_106, (void (*)(void))hook_entry_107, (void (*)(void))hook_entry_108, (void (*)(void))hook_entry_109, (void (*)(void))hook_entry_110, (void (*)(void))hook_entry_111, (void (*)(void))hook_entry_112, (void (*)(void))hook_entry_113, (void (*)(void))hook_entry_114, (void (*)(void))hook_entry_115, (void (*)(void))hook_entry_116, (void (*)(void))hook_entry_117, (void (*)(void))hook_entry_118, (void (*)(void))hook_entry_119, (void (*)(void))hook_entry_120, (void (*)(void))hook_entry_121, (void (*)(void))hook_entry_122, (void (*)(void))hook_entry_123, (void (*)(void))hook_entry_124, (void (*)(void))hook_entry_125, (void (*)(void))hook_entry_126, (void (*)(void))hook_entry_127, (void (*)(void))hook_entry_128, (void (*)(void))hook_entry_129, (void (*)(void))hook_entry_130, (void (*)(void))hook_entry_131, (void (*)(void))hook_entry_132, (void (*)(void))hook_entry_133, (void (*)(void))hook_entry_134, (void (*)(void))hook_entry_135, (void (*)(void))hook_entry_136, (void (*)(void))hook_entry_137, (void (*)(void))hook_entry_138, (void (*)(void))hook_entry_139, (void (*)(void))hook_entry_140, (void (*)(void))hook_entry_141, (void (*)(void))hook_entry_142, (void (*)(void))hook_entry_143, (void (*)(void))hook_entry_144, (void (*)(void))hook_entry_145, (void (*)(void))hook_entry_146, (void (*)(void))hook_entry_147, (void (*)(void))hook_entry_148, (void (*)(void))hook_entry_149, (void (*)(void))hook_entry_150, (void (*)(void))hook_entry_151, (void (*)(void))hook_entry_152, (void (*)(void))hook_entry_153, (void (*)(void))hook_entry_154, (void (*)(void))hook_entry_155, (void (*)(void))hook_entry_156, (void (*)(void))hook_entry_157, (void (*)(void))hook_entry_158, (void (*)(void))hook_entry_159, (void (*)(void))hook_entry_160, (void (*)(void))hook_entry_161, (void (*)(void))hook_entry_162, (void (*)(void))hook_entry_163, (void (*)(void))hook_entry_164, (void (*)(void))hook_entry_165, (void (*)(void))hook_entry_166, (void (*)(void))hook_entry_167, (void (*)(void))hook_entry_168, (void (*)(void))hook_entry_169, (void (*)(void))hook_entry_170, (void (*)(void))hook_entry_171, (void (*)(void))hook_entry_172, (void (*)(void))hook_entry_173, (void (*)(void))hook_entry_174, (void (*)(void))hook_entry_175, (void (*)(void))hook_entry_176, (void (*)(void))hook_entry_177, (void (*)(void))hook_entry_178, (void (*)(void))hook_entry_179, (void (*)(void))hook_entry_180, (void (*)(void))hook_entry_181, (void (*)(void))hook_entry_182, (void (*)(void))hook_entry_183, (void (*)(void))hook_entry_184, (void (*)(void))hook_entry_185, (void (*)(void))hook_entry_186, (void (*)(void))hook_entry_187, (void (*)(void))hook_entry_188, (void (*)(void))hook_entry_189, (void (*)(void))hook_entry_190, (void (*)(void))hook_entry_191, (void (*)(void))hook_entry_192, (void (*)(void))hook_entry_193, (void (*)(void))hook_entry_194, (void (*)(void))hook_entry_195, (void (*)(void))hook_entry_196, (void (*)(void))hook_entry_197, (void (*)(void))hook_entry_198, (void (*)(void))hook_entry_199, (void (*)(void))hook_entry_200, (void (*)(void))hook_entry_201, (void (*)(void))hook_entry_202, (void (*)(void))hook_entry_203, (void (*)(void))hook_entry_204, (void (*)(void))hook_entry_205, (void (*)(void))hook_entry_206, (void (*)(void))hook_entry_207, (void (*)(void))hook_entry_208, (void (*)(void))hook_entry_209, (void (*)(void))hook_entry_210, (void (*)(void))hook_entry_211, (void (*)(void))hook_entry_212, (void (*)(void))hook_entry_213, (void (*)(void))hook_entry_214, (void (*)(void))hook_entry_215, (void (*)(void))hook_entry_216, (void (*)(void))hook_entry_217, (void (*)(void))hook_entry_218, (void (*)(void))hook_entry_219, (void (*)(void))hook_entry_220, (void (*)(void))hook_entry_221, (void (*)(void))hook_entry_222, (void (*)(void))hook_entry_223, (void (*)(void))hook_entry_224, (void (*)(void))hook_entry_225, (void (*)(void))hook_entry_226, (void (*)(void))hook_entry_227, (void (*)(void))hook_entry_228, (void (*)(void))hook_entry_229, (void (*)(void))hook_entry_230, (void (*)(void))hook_entry_231, (void (*)(void))hook_entry_232, (void (*)(void))hook_entry_233, (void (*)(void))hook_entry_234, (void (*)(void))hook_entry_235, (void (*)(void))hook_entry_236, (void (*)(void))hook_entry_237, (void (*)(void))hook_entry_238, (void (*)(void))hook_entry_239, (void (*)(void))hook_entry_240, (void (*)(void))hook_entry_241, (void (*)(void))hook_entry_242, (void (*)(void))hook_entry_243, (void (*)(void))hook_entry_244, (void (*)(void))hook_entry_245, (void (*)(void))hook_entry_246, (void (*)(void))hook_entry_247, (void (*)(void))hook_entry_248, (void (*)(void))hook_entry_249, (void (*)(void))hook_entry_250, (void (*)(void))hook_entry_251, (void (*)(void))hook_entry_252, (void (*)(void))hook_entry_253, (void (*)(void))hook_entry_254, (void (*)(void))hook_entry_255 };
/* * NestedIntLib.h * * Created on: Dec 06, 2022 * Author: NoMaY * License: MIT */ #ifndef NESTEDINTLIB_H_ #define NESTEDINTLIB_H_ #define INTERRUPT___0 PERMIT #define INTERRUPT___1 PERMIT #define INTERRUPT___2 PERMIT #define INTERRUPT___3 PERMIT #define INTERRUPT___4 PERMIT #define INTERRUPT___5 PERMIT #define INTERRUPT___6 PERMIT #define INTERRUPT___7 PERMIT #define INTERRUPT___8 PERMIT #define INTERRUPT___9 PERMIT #define INTERRUPT__10 PERMIT #define INTERRUPT__11 PERMIT #define INTERRUPT__12 PERMIT #define INTERRUPT__13 PERMIT #define INTERRUPT__14 PERMIT #define INTERRUPT__15 PERMIT #define INTERRUPT__16 NOT_PERMIT // bus_error_isr #define INTERRUPT__17 PERMIT #define INTERRUPT__18 PERMIT #define INTERRUPT__19 PERMIT #define INTERRUPT__20 PERMIT #define INTERRUPT__21 PERMIT #define INTERRUPT__22 PERMIT #define INTERRUPT__23 PERMIT #define INTERRUPT__24 PERMIT #define INTERRUPT__25 PERMIT #define INTERRUPT__26 PERMIT #define INTERRUPT__27 PERMIT #define INTERRUPT__28 PERMIT #define INTERRUPT__29 PERMIT #define INTERRUPT__30 PERMIT #define INTERRUPT__31 PERMIT #define INTERRUPT__32 PERMIT #define INTERRUPT__33 PERMIT #define INTERRUPT__34 PERMIT #define INTERRUPT__35 PERMIT #define INTERRUPT__36 PERMIT #define INTERRUPT__37 PERMIT #define INTERRUPT__38 PERMIT #define INTERRUPT__39 PERMIT #define INTERRUPT__40 PERMIT #define INTERRUPT__41 PERMIT #define INTERRUPT__42 PERMIT #define INTERRUPT__43 PERMIT #define INTERRUPT__44 PERMIT #define INTERRUPT__45 PERMIT #define INTERRUPT__46 PERMIT #define INTERRUPT__47 PERMIT #define INTERRUPT__48 PERMIT #define INTERRUPT__49 PERMIT #define INTERRUPT__50 PERMIT #define INTERRUPT__51 PERMIT #define INTERRUPT__52 PERMIT #define INTERRUPT__53 PERMIT #define INTERRUPT__54 PERMIT #define INTERRUPT__55 PERMIT #define INTERRUPT__56 PERMIT #define INTERRUPT__57 PERMIT #define INTERRUPT__58 PERMIT #define INTERRUPT__59 PERMIT #define INTERRUPT__60 PERMIT #define INTERRUPT__61 PERMIT #define INTERRUPT__62 PERMIT #define INTERRUPT__63 PERMIT #define INTERRUPT__64 PERMIT #define INTERRUPT__65 PERMIT #define INTERRUPT__66 PERMIT #define INTERRUPT__67 PERMIT #define INTERRUPT__68 PERMIT #define INTERRUPT__69 PERMIT #define INTERRUPT__70 PERMIT #define INTERRUPT__71 PERMIT #define INTERRUPT__72 PERMIT #define INTERRUPT__73 PERMIT #define INTERRUPT__74 PERMIT #define INTERRUPT__75 PERMIT #define INTERRUPT__76 PERMIT #define INTERRUPT__77 PERMIT #define INTERRUPT__78 PERMIT #define INTERRUPT__79 PERMIT #define INTERRUPT__80 PERMIT #define INTERRUPT__81 PERMIT #define INTERRUPT__82 PERMIT #define INTERRUPT__83 PERMIT #define INTERRUPT__84 PERMIT #define INTERRUPT__85 PERMIT #define INTERRUPT__86 PERMIT #define INTERRUPT__87 PERMIT #define INTERRUPT__88 PERMIT #define INTERRUPT__89 PERMIT #define INTERRUPT__90 PERMIT #define INTERRUPT__91 PERMIT #define INTERRUPT__92 PERMIT #define INTERRUPT__93 PERMIT #define INTERRUPT__94 PERMIT #define INTERRUPT__95 PERMIT #define INTERRUPT__96 PERMIT #define INTERRUPT__97 PERMIT #define INTERRUPT__98 PERMIT #define INTERRUPT__99 PERMIT #define INTERRUPT_100 PERMIT #define INTERRUPT_101 PERMIT #define INTERRUPT_102 PERMIT #define INTERRUPT_103 PERMIT #define INTERRUPT_104 PERMIT #define INTERRUPT_105 PERMIT #define INTERRUPT_106 PERMIT #define INTERRUPT_107 PERMIT #define INTERRUPT_108 PERMIT #define INTERRUPT_109 PERMIT #define INTERRUPT_110 PERMIT #define INTERRUPT_111 PERMIT #define INTERRUPT_112 PERMIT #define INTERRUPT_113 PERMIT #define INTERRUPT_114 PERMIT #define INTERRUPT_115 PERMIT #define INTERRUPT_116 PERMIT #define INTERRUPT_117 PERMIT #define INTERRUPT_118 PERMIT #define INTERRUPT_119 PERMIT #define INTERRUPT_120 PERMIT #define INTERRUPT_121 PERMIT #define INTERRUPT_122 PERMIT #define INTERRUPT_123 PERMIT #define INTERRUPT_124 PERMIT #define INTERRUPT_125 PERMIT #define INTERRUPT_126 PERMIT #define INTERRUPT_127 PERMIT #define INTERRUPT_128 PERMIT #define INTERRUPT_129 PERMIT #define INTERRUPT_130 PERMIT #define INTERRUPT_131 PERMIT #define INTERRUPT_132 PERMIT #define INTERRUPT_133 PERMIT #define INTERRUPT_134 PERMIT #define INTERRUPT_135 PERMIT #define INTERRUPT_136 PERMIT #define INTERRUPT_137 PERMIT #define INTERRUPT_138 PERMIT #define INTERRUPT_139 PERMIT #define INTERRUPT_140 PERMIT #define INTERRUPT_141 PERMIT #define INTERRUPT_142 PERMIT #define INTERRUPT_143 PERMIT #define INTERRUPT_144 PERMIT #define INTERRUPT_145 PERMIT #define INTERRUPT_146 PERMIT #define INTERRUPT_147 PERMIT #define INTERRUPT_148 PERMIT #define INTERRUPT_149 PERMIT #define INTERRUPT_150 PERMIT #define INTERRUPT_151 PERMIT #define INTERRUPT_152 PERMIT #define INTERRUPT_153 PERMIT #define INTERRUPT_154 PERMIT #define INTERRUPT_155 PERMIT #define INTERRUPT_156 PERMIT #define INTERRUPT_157 PERMIT #define INTERRUPT_158 PERMIT #define INTERRUPT_159 PERMIT #define INTERRUPT_160 PERMIT #define INTERRUPT_161 PERMIT #define INTERRUPT_162 PERMIT #define INTERRUPT_163 PERMIT #define INTERRUPT_164 PERMIT #define INTERRUPT_165 PERMIT #define INTERRUPT_166 PERMIT #define INTERRUPT_167 PERMIT #define INTERRUPT_168 PERMIT #define INTERRUPT_169 PERMIT #define INTERRUPT_170 PERMIT #define INTERRUPT_171 PERMIT #define INTERRUPT_172 PERMIT #define INTERRUPT_173 PERMIT #define INTERRUPT_174 PERMIT #define INTERRUPT_175 PERMIT #define INTERRUPT_176 PERMIT #define INTERRUPT_177 PERMIT #define INTERRUPT_178 PERMIT #define INTERRUPT_179 PERMIT #define INTERRUPT_180 PERMIT #define INTERRUPT_181 PERMIT #define INTERRUPT_182 PERMIT #define INTERRUPT_183 PERMIT #define INTERRUPT_184 PERMIT #define INTERRUPT_185 PERMIT #define INTERRUPT_186 PERMIT #define INTERRUPT_187 PERMIT #define INTERRUPT_188 PERMIT #define INTERRUPT_189 PERMIT #define INTERRUPT_190 PERMIT #define INTERRUPT_191 PERMIT #define INTERRUPT_192 PERMIT #define INTERRUPT_193 PERMIT #define INTERRUPT_194 PERMIT #define INTERRUPT_195 PERMIT #define INTERRUPT_196 PERMIT #define INTERRUPT_197 PERMIT #define INTERRUPT_198 PERMIT #define INTERRUPT_199 PERMIT #define INTERRUPT_200 PERMIT #define INTERRUPT_201 PERMIT #define INTERRUPT_202 PERMIT #define INTERRUPT_203 PERMIT #define INTERRUPT_204 PERMIT #define INTERRUPT_205 PERMIT #define INTERRUPT_206 PERMIT #define INTERRUPT_207 PERMIT #define INTERRUPT_208 PERMIT #define INTERRUPT_209 PERMIT #define INTERRUPT_210 PERMIT #define INTERRUPT_211 PERMIT #define INTERRUPT_212 PERMIT #define INTERRUPT_213 PERMIT #define INTERRUPT_214 PERMIT #define INTERRUPT_215 PERMIT #define INTERRUPT_216 PERMIT #define INTERRUPT_217 PERMIT #define INTERRUPT_218 PERMIT #define INTERRUPT_219 PERMIT #define INTERRUPT_220 PERMIT #define INTERRUPT_221 PERMIT #define INTERRUPT_222 PERMIT #define INTERRUPT_223 PERMIT #define INTERRUPT_224 PERMIT #define INTERRUPT_225 PERMIT #define INTERRUPT_226 PERMIT #define INTERRUPT_227 PERMIT #define INTERRUPT_228 PERMIT #define INTERRUPT_229 PERMIT #define INTERRUPT_230 PERMIT #define INTERRUPT_231 PERMIT #define INTERRUPT_232 PERMIT #define INTERRUPT_233 PERMIT #define INTERRUPT_234 PERMIT #define INTERRUPT_235 PERMIT #define INTERRUPT_236 PERMIT #define INTERRUPT_237 PERMIT #define INTERRUPT_238 PERMIT #define INTERRUPT_239 PERMIT #define INTERRUPT_240 PERMIT #define INTERRUPT_241 PERMIT #define INTERRUPT_242 PERMIT #define INTERRUPT_243 PERMIT #define INTERRUPT_244 PERMIT #define INTERRUPT_245 PERMIT #define INTERRUPT_246 PERMIT #define INTERRUPT_247 PERMIT #define INTERRUPT_248 PERMIT #define INTERRUPT_249 PERMIT #define INTERRUPT_250 PERMIT #define INTERRUPT_251 PERMIT #define INTERRUPT_252 PERMIT #define INTERRUPT_253 PERMIT #define INTERRUPT_254 PERMIT #define INTERRUPT_255 PERMIT void NESTEDINTLIB_INT_HOOK_init(void); #endif /* NESTEDINTLIB_H_ */
/*********************************************************************** * * FILE : NestedIntLib_CCRX.c * DATE : 2022-12-06 * DESCRIPTION : Main Program * * NOTE:THIS IS A TYPICAL EXAMPLE. * ***********************************************************************/ #include "r_smc_entry.h" #include "NestedIntLib.h" void main(void); void main(void) { NESTEDINTLIB_INT_HOOK_init(); int_exception(16); // bus_error_isr set_ipl(BSP_CFG_FIT_IPL_MAX - 1); int_exception(0); // trap_isr set_ipl(BSP_CFG_FIT_IPL_MAX); int_exception(0); // trap_isr set_ipl(BSP_CFG_FIT_IPL_MAX + 1); int_exception(0); // trap_isr for(;;); } #pragma interrupt trap_isr(vect=0) void trap_isr(void) { nop(); }
こんにちは。NoMaYです。CC-RX版に加え、GNURX版とICCRX版も作ってみました。プロジェクトのファイル一式を以下のzipファイルに固めました。(なお、ICCRX版はルネサスRXシミュレータで命令レベルで本ライブラリのコードをステップ実行する場合に動作が極端に重くなる場所があります。要調査です。あと、それから、まだ実機では試していません。)issue_NestedIntLib_20221227.zip以下、肝心な部分のソースです。(肝心な部分は他にはありません。)NestedIntLib.c
/* * NestedIntLib.c * * Created on: Dec 06, 2022 * Last Modified on: Dec 27, 2022 * Author: NoMaY * License: MIT */ #include "r_smc_entry.h" #include "NestedIntLib.h" static void (* const Int_Hook_Vectors[])(void); void NESTEDINTLIB_INT_HOOK_init(void) { R_BSP_SET_INTB((void *)Int_Hook_Vectors); #if defined(__CCRX__) static void dummy_INT_COMMON_NESTEDINT_inline_asm(void); dummy_INT_COMMON_NESTEDINT_inline_asm(); #endif } // Convert `0xX` format --> `DD` format for CC-RX inline assembler. #if MY_BSP_CFG_UNNESTED_IPL_MAX >= 16 #error "MY_BSP_CFG_UNNESTED_IPL_MAX should be 0x0 - 0xF." #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 15 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 15 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 14 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 14 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 13 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 13 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 12 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 12 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 11 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 11 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 10 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 10 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 9 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 9 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 8 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 8 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 7 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 7 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 6 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 6 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 5 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 5 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 4 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 4 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 3 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 3 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 2 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 2 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 1 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 1 #elif MY_BSP_CFG_UNNESTED_IPL_MAX == 0 #define _MY_BSP_CFG_UNNESTED_IPL_MAX 0 #else #error "MY_BSP_CFG_UNNESTED_IPL_MAX should be 0x0 - 0xF." #endif #define R_BSP_ASM_TOKEN_SHARP # /* Just for convenience. */ #if defined(IMM) #undef IMM #endif #define IMM(imm) R_BSP_ASM_TOKEN_SHARP (imm) #if defined(ASM) #undef ASM #endif #define ASM R_BSP_ASM #if defined(LAB) #undef LAB #endif #define LAB R_BSP_ASM_LAB #if defined(LAB_NEXT) #undef LAB_NEXT #endif #define LAB_NEXT R_BSP_ASM_LAB_NEXT #if defined(LAB_PREV) #undef LAB_PREV #endif #define LAB_PREV R_BSP_ASM_LAB_PREV /* Miscellaneous. */ #if defined(INT_VECTORS) #undef INT_VECTORS #endif #if defined(STATIC_SYM) #undef STATIC_SYM #endif #if defined(__CCRX__) #define INT_VECTORS (TOPOF C$VECT) #define STATIC_SYM(sym_name) __$sym_name #define U_BSP_ASM_END_NAKED /* none */ #elif defined(__GNUC__) extern void * const rvectors_start[]; #define INT_VECTORS _rvectors_start #define STATIC_SYM(sym_name) _##sym_name #define U_BSP_ASM_END_NAKED ); #elif defined(__ICCRX__) extern void * const vector_table[]; #define INT_VECTORS _vector_table #define STATIC_SYM(sym_name) _##sym_name #define U_BSP_ASM_END_NAKED ); #endif #if defined(__CCRX__) static void dummy_INT_COMMON_NESTEDINT_inline_asm(void) { // To prevent developers from being misled regarding the following inline assemble errors. // E0552111:Symbol is undefined // E0552113:Symbol definition is not appropriate // E0552052:Addressing mode specifier is not appropriate // or various inline assemble errors return; } #endif R_BSP_PRAGMA_STATIC_INLINE_ASM( INT_COMMON_NESTEDINT_PERMIT ) void INT_COMMON_NESTEDINT_PERMIT(void) { R_BSP_ASM_BEGIN ASM( PUSH.L R1 ) // if(MY_BSP_CFG_UNNESTED_IPL_MAX > (((R_BSP_GET_PSW()) >> 24) & 0xF)) // { // R_BSP_SET_IPL(MY_BSP_CFG_UNNESTED_IPL_MAX); // } // R_BSP_SETPSW_I(); ASM( MVFC PSW, R1 ) #ifdef __RXV3 ASM( BFMOVZ IMM(24), IMM(0), IMM(4), R1, R1 ) #else ASM( SHLR IMM(24), R1 ) ASM( AND IMM(15), R1 ) #endif ASM( CMP IMM(_MY_BSP_CFG_UNNESTED_IPL_MAX), R1 ) ASM( BGEU LAB_NEXT(1) ) ASM( MVTIPL IMM(_MY_BSP_CFG_UNNESTED_IPL_MAX) ) LAB(1:) ASM( SETPSW I ) ASM( MOV.L 4[R0], R1 ) // address of hook_entry_XXX + 3 --> R1 // 3 = size of BSR.W ASM( ADD IMM(INT_VECTORS - (STATIC_SYM( hook_entry___0 ) + 3)), R1 ) // 3 = size of BSR.W ASM( MOV.L [R1], 4[R0] ) ASM( RTSD R_BSP_ASM_TOKEN_SHARP 4, R1-R1 ) // i.e. POP R1, JMP [SP+] U_BSP_ASM_END_NAKED } R_BSP_PRAGMA_STATIC_INLINE_ASM( INT_COMMON_NESTEDINT_NOT_PERMIT ) void INT_COMMON_NESTEDINT_NOT_PERMIT(void) { R_BSP_ASM_BEGIN ASM( PUSH.L R1 ) ASM( MOV.L 4[R0], R1 ) // address of hook_entry_XXX + 3 --> R1 // 3 = size of BSR.W ASM( ADD IMM(INT_VECTORS - (STATIC_SYM( hook_entry___0 ) + 3)), R1 ) // 3 = size of BSR.W ASM( MOV.L [R1], 4[R0] ) ASM( RTSD IMM(4), R1-R1 ) // i.e. POP R1, JMP [SP+] U_BSP_ASM_END_NAKED } #if defined(__CCRX__) R_BSP_PRAGMA_STATIC_INLINE_ASM( INT_ENTRY_NESTEDINT_PERMIT ) #else R_BSP_PRAGMA_STATIC_INLINE( INT_ENTRY_NESTEDINT_PERMIT ) #endif void INT_ENTRY_NESTEDINT_PERMIT(void) { R_BSP_ASM_BEGIN ASM( BSR.W STATIC_SYM( INT_COMMON_NESTEDINT_PERMIT ) ) U_BSP_ASM_END_NAKED } #if defined(__CCRX__) R_BSP_PRAGMA_STATIC_INLINE_ASM( INT_ENTRY_NESTEDINT_NOT_PERMIT ) #else R_BSP_PRAGMA_STATIC_INLINE( INT_ENTRY_NESTEDINT_NOT_PERMIT ) #endif void INT_ENTRY_NESTEDINT_NOT_PERMIT(void) { R_BSP_ASM_BEGIN ASM( BSR.W STATIC_SYM( INT_COMMON_NESTEDINT_NOT_PERMIT ) ) U_BSP_ASM_END_NAKED } // Documents // English // https://www.renesas.com/us/en/document/mas/rx-family-rxv1-instruction-set-architecture-users-manual-software-rev130 // https://www.renesas.com/us/en/document/mas/rx-family-rxv2-instruction-set-architecture-users-manual-software // https://www.renesas.com/us/en/document/mas/rx-family-rxv3-instruction-set-architecture-users-manual-software-rev100 // Japanese // https://www.renesas.com/jp/ja/document/mas/rx-family-rxv1-instruction-set-architecture-users-manual-software-rev130 // https://www.renesas.com/jp/ja/document/mas/rx-family-rxv2-instruction-set-architecture-users-manual-software // https://www.renesas.com/jp/ja/document/mas/rx-family-rxv3-instruction-set-architecture-users-manual-software-rev100 #if defined(__CCRX__) // To prevent the symbol from being optimized out. void * const dummy_INT_COMMON_NESTEDINT_PERMIT = (void *)INT_COMMON_NESTEDINT_PERMIT; void * const dummy_INT_COMMON_NESTEDINT_NOT_PERMIT = (void *)INT_COMMON_NESTEDINT_NOT_PERMIT; // To prevent the section name symbol `C$VECT` from being optimized out. void * const dummy_VECTTBL = (void *)__sectop("C$VECT"); #elif defined(__GNUC__) // To prevent the symbol from being optimized out. static void INT_COMMON_NESTEDINT_PERMIT(void) __attribute__((used)); static void INT_COMMON_NESTEDINT_NOT_PERMIT(void) __attribute__((used)); #elif defined(__ICCRX__) // To prevent the symbol from being optimized out. #pragma required=INT_COMMON_NESTEDINT_PERMIT #pragma required=INT_COMMON_NESTEDINT_NOT_PERMIT #pragma required=vector_table #endif // The code size of the following functions is just 4 bytes. // For PERMIT // 00000000 39rrrr W BSR.W STATIC_SYMBOL( INT_COMMON_NESTEDINT_PERMIT ) // 00000003 02 RTS // Not used. // For NOT_PERMIT // 00000000 39rrrr W BSR.W STATIC_SYMBOL( INT_COMMON_NESTEDINT_NOT_PERMIT ) // 00000003 02 RTS // Not used. #define _INT_ENTRY(sel) INT_ENTRY_NESTEDINT_##sel() #define INT_ENTRY(sel) _INT_ENTRY(sel) static void hook_entry___0(void) { INT_ENTRY(INTERRUPT___0); } static void hook_entry___1(void) { INT_ENTRY(INTERRUPT___1); } static void hook_entry___2(void) { INT_ENTRY(INTERRUPT___2); } static void hook_entry___3(void) { INT_ENTRY(INTERRUPT___3); } static void hook_entry___4(void) { INT_ENTRY(INTERRUPT___4); } static void hook_entry___5(void) { INT_ENTRY(INTERRUPT___5); } static void hook_entry___6(void) { INT_ENTRY(INTERRUPT___6); } static void hook_entry___7(void) { INT_ENTRY(INTERRUPT___7); } static void hook_entry___8(void) { INT_ENTRY(INTERRUPT___8); } static void hook_entry___9(void) { INT_ENTRY(INTERRUPT___9); } static void hook_entry__10(void) { INT_ENTRY(INTERRUPT__10); } static void hook_entry__11(void) { INT_ENTRY(INTERRUPT__11); } static void hook_entry__12(void) { INT_ENTRY(INTERRUPT__12); } static void hook_entry__13(void) { INT_ENTRY(INTERRUPT__13); } static void hook_entry__14(void) { INT_ENTRY(INTERRUPT__14); } static void hook_entry__15(void) { INT_ENTRY(INTERRUPT__15); } static void hook_entry__16(void) { INT_ENTRY(INTERRUPT__16); } static void hook_entry__17(void) { INT_ENTRY(INTERRUPT__17); } static void hook_entry__18(void) { INT_ENTRY(INTERRUPT__18); } static void hook_entry__19(void) { INT_ENTRY(INTERRUPT__19); } static void hook_entry__20(void) { INT_ENTRY(INTERRUPT__20); } static void hook_entry__21(void) { INT_ENTRY(INTERRUPT__21); } static void hook_entry__22(void) { INT_ENTRY(INTERRUPT__22); } static void hook_entry__23(void) { INT_ENTRY(INTERRUPT__23); } static void hook_entry__24(void) { INT_ENTRY(INTERRUPT__24); } static void hook_entry__25(void) { INT_ENTRY(INTERRUPT__25); } static void hook_entry__26(void) { INT_ENTRY(INTERRUPT__26); } static void hook_entry__27(void) { INT_ENTRY(INTERRUPT__27); } static void hook_entry__28(void) { INT_ENTRY(INTERRUPT__28); } static void hook_entry__29(void) { INT_ENTRY(INTERRUPT__29); } static void hook_entry__30(void) { INT_ENTRY(INTERRUPT__30); } static void hook_entry__31(void) { INT_ENTRY(INTERRUPT__31); } static void hook_entry__32(void) { INT_ENTRY(INTERRUPT__32); } static void hook_entry__33(void) { INT_ENTRY(INTERRUPT__33); } static void hook_entry__34(void) { INT_ENTRY(INTERRUPT__34); } static void hook_entry__35(void) { INT_ENTRY(INTERRUPT__35); } static void hook_entry__36(void) { INT_ENTRY(INTERRUPT__36); } static void hook_entry__37(void) { INT_ENTRY(INTERRUPT__37); } static void hook_entry__38(void) { INT_ENTRY(INTERRUPT__38); } static void hook_entry__39(void) { INT_ENTRY(INTERRUPT__39); } static void hook_entry__40(void) { INT_ENTRY(INTERRUPT__40); } static void hook_entry__41(void) { INT_ENTRY(INTERRUPT__41); } static void hook_entry__42(void) { INT_ENTRY(INTERRUPT__42); } static void hook_entry__43(void) { INT_ENTRY(INTERRUPT__43); } static void hook_entry__44(void) { INT_ENTRY(INTERRUPT__44); } static void hook_entry__45(void) { INT_ENTRY(INTERRUPT__45); } static void hook_entry__46(void) { INT_ENTRY(INTERRUPT__46); } static void hook_entry__47(void) { INT_ENTRY(INTERRUPT__47); } static void hook_entry__48(void) { INT_ENTRY(INTERRUPT__48); } static void hook_entry__49(void) { INT_ENTRY(INTERRUPT__49); } static void hook_entry__50(void) { INT_ENTRY(INTERRUPT__50); } static void hook_entry__51(void) { INT_ENTRY(INTERRUPT__51); } static void hook_entry__52(void) { INT_ENTRY(INTERRUPT__52); } static void hook_entry__53(void) { INT_ENTRY(INTERRUPT__53); } static void hook_entry__54(void) { INT_ENTRY(INTERRUPT__54); } static void hook_entry__55(void) { INT_ENTRY(INTERRUPT__55); } static void hook_entry__56(void) { INT_ENTRY(INTERRUPT__56); } static void hook_entry__57(void) { INT_ENTRY(INTERRUPT__57); } static void hook_entry__58(void) { INT_ENTRY(INTERRUPT__58); } static void hook_entry__59(void) { INT_ENTRY(INTERRUPT__59); } static void hook_entry__60(void) { INT_ENTRY(INTERRUPT__60); } static void hook_entry__61(void) { INT_ENTRY(INTERRUPT__61); } static void hook_entry__62(void) { INT_ENTRY(INTERRUPT__62); } static void hook_entry__63(void) { INT_ENTRY(INTERRUPT__63); } static void hook_entry__64(void) { INT_ENTRY(INTERRUPT__64); } static void hook_entry__65(void) { INT_ENTRY(INTERRUPT__65); } static void hook_entry__66(void) { INT_ENTRY(INTERRUPT__66); } static void hook_entry__67(void) { INT_ENTRY(INTERRUPT__67); } static void hook_entry__68(void) { INT_ENTRY(INTERRUPT__68); } static void hook_entry__69(void) { INT_ENTRY(INTERRUPT__69); } static void hook_entry__70(void) { INT_ENTRY(INTERRUPT__70); } static void hook_entry__71(void) { INT_ENTRY(INTERRUPT__71); } static void hook_entry__72(void) { INT_ENTRY(INTERRUPT__72); } static void hook_entry__73(void) { INT_ENTRY(INTERRUPT__73); } static void hook_entry__74(void) { INT_ENTRY(INTERRUPT__74); } static void hook_entry__75(void) { INT_ENTRY(INTERRUPT__75); } static void hook_entry__76(void) { INT_ENTRY(INTERRUPT__76); } static void hook_entry__77(void) { INT_ENTRY(INTERRUPT__77); } static void hook_entry__78(void) { INT_ENTRY(INTERRUPT__78); } static void hook_entry__79(void) { INT_ENTRY(INTERRUPT__79); } static void hook_entry__80(void) { INT_ENTRY(INTERRUPT__80); } static void hook_entry__81(void) { INT_ENTRY(INTERRUPT__81); } static void hook_entry__82(void) { INT_ENTRY(INTERRUPT__82); } static void hook_entry__83(void) { INT_ENTRY(INTERRUPT__83); } static void hook_entry__84(void) { INT_ENTRY(INTERRUPT__84); } static void hook_entry__85(void) { INT_ENTRY(INTERRUPT__85); } static void hook_entry__86(void) { INT_ENTRY(INTERRUPT__86); } static void hook_entry__87(void) { INT_ENTRY(INTERRUPT__87); } static void hook_entry__88(void) { INT_ENTRY(INTERRUPT__88); } static void hook_entry__89(void) { INT_ENTRY(INTERRUPT__89); } static void hook_entry__90(void) { INT_ENTRY(INTERRUPT__90); } static void hook_entry__91(void) { INT_ENTRY(INTERRUPT__91); } static void hook_entry__92(void) { INT_ENTRY(INTERRUPT__92); } static void hook_entry__93(void) { INT_ENTRY(INTERRUPT__93); } static void hook_entry__94(void) { INT_ENTRY(INTERRUPT__94); } static void hook_entry__95(void) { INT_ENTRY(INTERRUPT__95); } static void hook_entry__96(void) { INT_ENTRY(INTERRUPT__96); } static void hook_entry__97(void) { INT_ENTRY(INTERRUPT__97); } static void hook_entry__98(void) { INT_ENTRY(INTERRUPT__98); } static void hook_entry__99(void) { INT_ENTRY(INTERRUPT__99); } static void hook_entry_100(void) { INT_ENTRY(INTERRUPT_100); } static void hook_entry_101(void) { INT_ENTRY(INTERRUPT_101); } static void hook_entry_102(void) { INT_ENTRY(INTERRUPT_102); } static void hook_entry_103(void) { INT_ENTRY(INTERRUPT_103); } static void hook_entry_104(void) { INT_ENTRY(INTERRUPT_104); } static void hook_entry_105(void) { INT_ENTRY(INTERRUPT_105); } static void hook_entry_106(void) { INT_ENTRY(INTERRUPT_106); } static void hook_entry_107(void) { INT_ENTRY(INTERRUPT_107); } static void hook_entry_108(void) { INT_ENTRY(INTERRUPT_108); } static void hook_entry_109(void) { INT_ENTRY(INTERRUPT_109); } static void hook_entry_110(void) { INT_ENTRY(INTERRUPT_110); } static void hook_entry_111(void) { INT_ENTRY(INTERRUPT_111); } static void hook_entry_112(void) { INT_ENTRY(INTERRUPT_112); } static void hook_entry_113(void) { INT_ENTRY(INTERRUPT_113); } static void hook_entry_114(void) { INT_ENTRY(INTERRUPT_114); } static void hook_entry_115(void) { INT_ENTRY(INTERRUPT_115); } static void hook_entry_116(void) { INT_ENTRY(INTERRUPT_116); } static void hook_entry_117(void) { INT_ENTRY(INTERRUPT_117); } static void hook_entry_118(void) { INT_ENTRY(INTERRUPT_118); } static void hook_entry_119(void) { INT_ENTRY(INTERRUPT_119); } static void hook_entry_120(void) { INT_ENTRY(INTERRUPT_120); } static void hook_entry_121(void) { INT_ENTRY(INTERRUPT_121); } static void hook_entry_122(void) { INT_ENTRY(INTERRUPT_122); } static void hook_entry_123(void) { INT_ENTRY(INTERRUPT_123); } static void hook_entry_124(void) { INT_ENTRY(INTERRUPT_124); } static void hook_entry_125(void) { INT_ENTRY(INTERRUPT_125); } static void hook_entry_126(void) { INT_ENTRY(INTERRUPT_126); } static void hook_entry_127(void) { INT_ENTRY(INTERRUPT_127); } static void hook_entry_128(void) { INT_ENTRY(INTERRUPT_128); } static void hook_entry_129(void) { INT_ENTRY(INTERRUPT_129); } static void hook_entry_130(void) { INT_ENTRY(INTERRUPT_130); } static void hook_entry_131(void) { INT_ENTRY(INTERRUPT_131); } static void hook_entry_132(void) { INT_ENTRY(INTERRUPT_132); } static void hook_entry_133(void) { INT_ENTRY(INTERRUPT_133); } static void hook_entry_134(void) { INT_ENTRY(INTERRUPT_134); } static void hook_entry_135(void) { INT_ENTRY(INTERRUPT_135); } static void hook_entry_136(void) { INT_ENTRY(INTERRUPT_136); } static void hook_entry_137(void) { INT_ENTRY(INTERRUPT_137); } static void hook_entry_138(void) { INT_ENTRY(INTERRUPT_138); } static void hook_entry_139(void) { INT_ENTRY(INTERRUPT_139); } static void hook_entry_140(void) { INT_ENTRY(INTERRUPT_140); } static void hook_entry_141(void) { INT_ENTRY(INTERRUPT_141); } static void hook_entry_142(void) { INT_ENTRY(INTERRUPT_142); } static void hook_entry_143(void) { INT_ENTRY(INTERRUPT_143); } static void hook_entry_144(void) { INT_ENTRY(INTERRUPT_144); } static void hook_entry_145(void) { INT_ENTRY(INTERRUPT_145); } static void hook_entry_146(void) { INT_ENTRY(INTERRUPT_146); } static void hook_entry_147(void) { INT_ENTRY(INTERRUPT_147); } static void hook_entry_148(void) { INT_ENTRY(INTERRUPT_148); } static void hook_entry_149(void) { INT_ENTRY(INTERRUPT_149); } static void hook_entry_150(void) { INT_ENTRY(INTERRUPT_150); } static void hook_entry_151(void) { INT_ENTRY(INTERRUPT_151); } static void hook_entry_152(void) { INT_ENTRY(INTERRUPT_152); } static void hook_entry_153(void) { INT_ENTRY(INTERRUPT_153); } static void hook_entry_154(void) { INT_ENTRY(INTERRUPT_154); } static void hook_entry_155(void) { INT_ENTRY(INTERRUPT_155); } static void hook_entry_156(void) { INT_ENTRY(INTERRUPT_156); } static void hook_entry_157(void) { INT_ENTRY(INTERRUPT_157); } static void hook_entry_158(void) { INT_ENTRY(INTERRUPT_158); } static void hook_entry_159(void) { INT_ENTRY(INTERRUPT_159); } static void hook_entry_160(void) { INT_ENTRY(INTERRUPT_160); } static void hook_entry_161(void) { INT_ENTRY(INTERRUPT_161); } static void hook_entry_162(void) { INT_ENTRY(INTERRUPT_162); } static void hook_entry_163(void) { INT_ENTRY(INTERRUPT_163); } static void hook_entry_164(void) { INT_ENTRY(INTERRUPT_164); } static void hook_entry_165(void) { INT_ENTRY(INTERRUPT_165); } static void hook_entry_166(void) { INT_ENTRY(INTERRUPT_166); } static void hook_entry_167(void) { INT_ENTRY(INTERRUPT_167); } static void hook_entry_168(void) { INT_ENTRY(INTERRUPT_168); } static void hook_entry_169(void) { INT_ENTRY(INTERRUPT_169); } static void hook_entry_170(void) { INT_ENTRY(INTERRUPT_170); } static void hook_entry_171(void) { INT_ENTRY(INTERRUPT_171); } static void hook_entry_172(void) { INT_ENTRY(INTERRUPT_172); } static void hook_entry_173(void) { INT_ENTRY(INTERRUPT_173); } static void hook_entry_174(void) { INT_ENTRY(INTERRUPT_174); } static void hook_entry_175(void) { INT_ENTRY(INTERRUPT_175); } static void hook_entry_176(void) { INT_ENTRY(INTERRUPT_176); } static void hook_entry_177(void) { INT_ENTRY(INTERRUPT_177); } static void hook_entry_178(void) { INT_ENTRY(INTERRUPT_178); } static void hook_entry_179(void) { INT_ENTRY(INTERRUPT_179); } static void hook_entry_180(void) { INT_ENTRY(INTERRUPT_180); } static void hook_entry_181(void) { INT_ENTRY(INTERRUPT_181); } static void hook_entry_182(void) { INT_ENTRY(INTERRUPT_182); } static void hook_entry_183(void) { INT_ENTRY(INTERRUPT_183); } static void hook_entry_184(void) { INT_ENTRY(INTERRUPT_184); } static void hook_entry_185(void) { INT_ENTRY(INTERRUPT_185); } static void hook_entry_186(void) { INT_ENTRY(INTERRUPT_186); } static void hook_entry_187(void) { INT_ENTRY(INTERRUPT_187); } static void hook_entry_188(void) { INT_ENTRY(INTERRUPT_188); } static void hook_entry_189(void) { INT_ENTRY(INTERRUPT_189); } static void hook_entry_190(void) { INT_ENTRY(INTERRUPT_190); } static void hook_entry_191(void) { INT_ENTRY(INTERRUPT_191); } static void hook_entry_192(void) { INT_ENTRY(INTERRUPT_192); } static void hook_entry_193(void) { INT_ENTRY(INTERRUPT_193); } static void hook_entry_194(void) { INT_ENTRY(INTERRUPT_194); } static void hook_entry_195(void) { INT_ENTRY(INTERRUPT_195); } static void hook_entry_196(void) { INT_ENTRY(INTERRUPT_196); } static void hook_entry_197(void) { INT_ENTRY(INTERRUPT_197); } static void hook_entry_198(void) { INT_ENTRY(INTERRUPT_198); } static void hook_entry_199(void) { INT_ENTRY(INTERRUPT_199); } static void hook_entry_200(void) { INT_ENTRY(INTERRUPT_200); } static void hook_entry_201(void) { INT_ENTRY(INTERRUPT_201); } static void hook_entry_202(void) { INT_ENTRY(INTERRUPT_202); } static void hook_entry_203(void) { INT_ENTRY(INTERRUPT_203); } static void hook_entry_204(void) { INT_ENTRY(INTERRUPT_204); } static void hook_entry_205(void) { INT_ENTRY(INTERRUPT_205); } static void hook_entry_206(void) { INT_ENTRY(INTERRUPT_206); } static void hook_entry_207(void) { INT_ENTRY(INTERRUPT_207); } static void hook_entry_208(void) { INT_ENTRY(INTERRUPT_208); } static void hook_entry_209(void) { INT_ENTRY(INTERRUPT_209); } static void hook_entry_210(void) { INT_ENTRY(INTERRUPT_210); } static void hook_entry_211(void) { INT_ENTRY(INTERRUPT_211); } static void hook_entry_212(void) { INT_ENTRY(INTERRUPT_212); } static void hook_entry_213(void) { INT_ENTRY(INTERRUPT_213); } static void hook_entry_214(void) { INT_ENTRY(INTERRUPT_214); } static void hook_entry_215(void) { INT_ENTRY(INTERRUPT_215); } static void hook_entry_216(void) { INT_ENTRY(INTERRUPT_216); } static void hook_entry_217(void) { INT_ENTRY(INTERRUPT_217); } static void hook_entry_218(void) { INT_ENTRY(INTERRUPT_218); } static void hook_entry_219(void) { INT_ENTRY(INTERRUPT_219); } static void hook_entry_220(void) { INT_ENTRY(INTERRUPT_220); } static void hook_entry_221(void) { INT_ENTRY(INTERRUPT_221); } static void hook_entry_222(void) { INT_ENTRY(INTERRUPT_222); } static void hook_entry_223(void) { INT_ENTRY(INTERRUPT_223); } static void hook_entry_224(void) { INT_ENTRY(INTERRUPT_224); } static void hook_entry_225(void) { INT_ENTRY(INTERRUPT_225); } static void hook_entry_226(void) { INT_ENTRY(INTERRUPT_226); } static void hook_entry_227(void) { INT_ENTRY(INTERRUPT_227); } static void hook_entry_228(void) { INT_ENTRY(INTERRUPT_228); } static void hook_entry_229(void) { INT_ENTRY(INTERRUPT_229); } static void hook_entry_230(void) { INT_ENTRY(INTERRUPT_230); } static void hook_entry_231(void) { INT_ENTRY(INTERRUPT_231); } static void hook_entry_232(void) { INT_ENTRY(INTERRUPT_232); } static void hook_entry_233(void) { INT_ENTRY(INTERRUPT_233); } static void hook_entry_234(void) { INT_ENTRY(INTERRUPT_234); } static void hook_entry_235(void) { INT_ENTRY(INTERRUPT_235); } static void hook_entry_236(void) { INT_ENTRY(INTERRUPT_236); } static void hook_entry_237(void) { INT_ENTRY(INTERRUPT_237); } static void hook_entry_238(void) { INT_ENTRY(INTERRUPT_238); } static void hook_entry_239(void) { INT_ENTRY(INTERRUPT_239); } static void hook_entry_240(void) { INT_ENTRY(INTERRUPT_240); } static void hook_entry_241(void) { INT_ENTRY(INTERRUPT_241); } static void hook_entry_242(void) { INT_ENTRY(INTERRUPT_242); } static void hook_entry_243(void) { INT_ENTRY(INTERRUPT_243); } static void hook_entry_244(void) { INT_ENTRY(INTERRUPT_244); } static void hook_entry_245(void) { INT_ENTRY(INTERRUPT_245); } static void hook_entry_246(void) { INT_ENTRY(INTERRUPT_246); } static void hook_entry_247(void) { INT_ENTRY(INTERRUPT_247); } static void hook_entry_248(void) { INT_ENTRY(INTERRUPT_248); } static void hook_entry_249(void) { INT_ENTRY(INTERRUPT_249); } static void hook_entry_250(void) { INT_ENTRY(INTERRUPT_250); } static void hook_entry_251(void) { INT_ENTRY(INTERRUPT_251); } static void hook_entry_252(void) { INT_ENTRY(INTERRUPT_252); } static void hook_entry_253(void) { INT_ENTRY(INTERRUPT_253); } static void hook_entry_254(void) { INT_ENTRY(INTERRUPT_254); } static void hook_entry_255(void) { INT_ENTRY(INTERRUPT_255); } static void (* const Int_Hook_Vectors[])(void) = { (void (*)(void))hook_entry___0, (void (*)(void))hook_entry___1, (void (*)(void))hook_entry___2, (void (*)(void))hook_entry___3, (void (*)(void))hook_entry___4, (void (*)(void))hook_entry___5, (void (*)(void))hook_entry___6, (void (*)(void))hook_entry___7, (void (*)(void))hook_entry___8, (void (*)(void))hook_entry___9, (void (*)(void))hook_entry__10, (void (*)(void))hook_entry__11, (void (*)(void))hook_entry__12, (void (*)(void))hook_entry__13, (void (*)(void))hook_entry__14, (void (*)(void))hook_entry__15, (void (*)(void))hook_entry__16, (void (*)(void))hook_entry__17, (void (*)(void))hook_entry__18, (void (*)(void))hook_entry__19, (void (*)(void))hook_entry__20, (void (*)(void))hook_entry__21, (void (*)(void))hook_entry__22, (void (*)(void))hook_entry__23, (void (*)(void))hook_entry__24, (void (*)(void))hook_entry__25, (void (*)(void))hook_entry__26, (void (*)(void))hook_entry__27, (void (*)(void))hook_entry__28, (void (*)(void))hook_entry__29, (void (*)(void))hook_entry__30, (void (*)(void))hook_entry__31, (void (*)(void))hook_entry__32, (void (*)(void))hook_entry__33, (void (*)(void))hook_entry__34, (void (*)(void))hook_entry__35, (void (*)(void))hook_entry__36, (void (*)(void))hook_entry__37, (void (*)(void))hook_entry__38, (void (*)(void))hook_entry__39, (void (*)(void))hook_entry__40, (void (*)(void))hook_entry__41, (void (*)(void))hook_entry__42, (void (*)(void))hook_entry__43, (void (*)(void))hook_entry__44, (void (*)(void))hook_entry__45, (void (*)(void))hook_entry__46, (void (*)(void))hook_entry__47, (void (*)(void))hook_entry__48, (void (*)(void))hook_entry__49, (void (*)(void))hook_entry__50, (void (*)(void))hook_entry__51, (void (*)(void))hook_entry__52, (void (*)(void))hook_entry__53, (void (*)(void))hook_entry__54, (void (*)(void))hook_entry__55, (void (*)(void))hook_entry__56, (void (*)(void))hook_entry__57, (void (*)(void))hook_entry__58, (void (*)(void))hook_entry__59, (void (*)(void))hook_entry__60, (void (*)(void))hook_entry__61, (void (*)(void))hook_entry__62, (void (*)(void))hook_entry__63, (void (*)(void))hook_entry__64, (void (*)(void))hook_entry__65, (void (*)(void))hook_entry__66, (void (*)(void))hook_entry__67, (void (*)(void))hook_entry__68, (void (*)(void))hook_entry__69, (void (*)(void))hook_entry__70, (void (*)(void))hook_entry__71, (void (*)(void))hook_entry__72, (void (*)(void))hook_entry__73, (void (*)(void))hook_entry__74, (void (*)(void))hook_entry__75, (void (*)(void))hook_entry__76, (void (*)(void))hook_entry__77, (void (*)(void))hook_entry__78, (void (*)(void))hook_entry__79, (void (*)(void))hook_entry__80, (void (*)(void))hook_entry__81, (void (*)(void))hook_entry__82, (void (*)(void))hook_entry__83, (void (*)(void))hook_entry__84, (void (*)(void))hook_entry__85, (void (*)(void))hook_entry__86, (void (*)(void))hook_entry__87, (void (*)(void))hook_entry__88, (void (*)(void))hook_entry__89, (void (*)(void))hook_entry__90, (void (*)(void))hook_entry__91, (void (*)(void))hook_entry__92, (void (*)(void))hook_entry__93, (void (*)(void))hook_entry__94, (void (*)(void))hook_entry__95, (void (*)(void))hook_entry__96, (void (*)(void))hook_entry__97, (void (*)(void))hook_entry__98, (void (*)(void))hook_entry__99, (void (*)(void))hook_entry_100, (void (*)(void))hook_entry_101, (void (*)(void))hook_entry_102, (void (*)(void))hook_entry_103, (void (*)(void))hook_entry_104, (void (*)(void))hook_entry_105, (void (*)(void))hook_entry_106, (void (*)(void))hook_entry_107, (void (*)(void))hook_entry_108, (void (*)(void))hook_entry_109, (void (*)(void))hook_entry_110, (void (*)(void))hook_entry_111, (void (*)(void))hook_entry_112, (void (*)(void))hook_entry_113, (void (*)(void))hook_entry_114, (void (*)(void))hook_entry_115, (void (*)(void))hook_entry_116, (void (*)(void))hook_entry_117, (void (*)(void))hook_entry_118, (void (*)(void))hook_entry_119, (void (*)(void))hook_entry_120, (void (*)(void))hook_entry_121, (void (*)(void))hook_entry_122, (void (*)(void))hook_entry_123, (void (*)(void))hook_entry_124, (void (*)(void))hook_entry_125, (void (*)(void))hook_entry_126, (void (*)(void))hook_entry_127, (void (*)(void))hook_entry_128, (void (*)(void))hook_entry_129, (void (*)(void))hook_entry_130, (void (*)(void))hook_entry_131, (void (*)(void))hook_entry_132, (void (*)(void))hook_entry_133, (void (*)(void))hook_entry_134, (void (*)(void))hook_entry_135, (void (*)(void))hook_entry_136, (void (*)(void))hook_entry_137, (void (*)(void))hook_entry_138, (void (*)(void))hook_entry_139, (void (*)(void))hook_entry_140, (void (*)(void))hook_entry_141, (void (*)(void))hook_entry_142, (void (*)(void))hook_entry_143, (void (*)(void))hook_entry_144, (void (*)(void))hook_entry_145, (void (*)(void))hook_entry_146, (void (*)(void))hook_entry_147, (void (*)(void))hook_entry_148, (void (*)(void))hook_entry_149, (void (*)(void))hook_entry_150, (void (*)(void))hook_entry_151, (void (*)(void))hook_entry_152, (void (*)(void))hook_entry_153, (void (*)(void))hook_entry_154, (void (*)(void))hook_entry_155, (void (*)(void))hook_entry_156, (void (*)(void))hook_entry_157, (void (*)(void))hook_entry_158, (void (*)(void))hook_entry_159, (void (*)(void))hook_entry_160, (void (*)(void))hook_entry_161, (void (*)(void))hook_entry_162, (void (*)(void))hook_entry_163, (void (*)(void))hook_entry_164, (void (*)(void))hook_entry_165, (void (*)(void))hook_entry_166, (void (*)(void))hook_entry_167, (void (*)(void))hook_entry_168, (void (*)(void))hook_entry_169, (void (*)(void))hook_entry_170, (void (*)(void))hook_entry_171, (void (*)(void))hook_entry_172, (void (*)(void))hook_entry_173, (void (*)(void))hook_entry_174, (void (*)(void))hook_entry_175, (void (*)(void))hook_entry_176, (void (*)(void))hook_entry_177, (void (*)(void))hook_entry_178, (void (*)(void))hook_entry_179, (void (*)(void))hook_entry_180, (void (*)(void))hook_entry_181, (void (*)(void))hook_entry_182, (void (*)(void))hook_entry_183, (void (*)(void))hook_entry_184, (void (*)(void))hook_entry_185, (void (*)(void))hook_entry_186, (void (*)(void))hook_entry_187, (void (*)(void))hook_entry_188, (void (*)(void))hook_entry_189, (void (*)(void))hook_entry_190, (void (*)(void))hook_entry_191, (void (*)(void))hook_entry_192, (void (*)(void))hook_entry_193, (void (*)(void))hook_entry_194, (void (*)(void))hook_entry_195, (void (*)(void))hook_entry_196, (void (*)(void))hook_entry_197, (void (*)(void))hook_entry_198, (void (*)(void))hook_entry_199, (void (*)(void))hook_entry_200, (void (*)(void))hook_entry_201, (void (*)(void))hook_entry_202, (void (*)(void))hook_entry_203, (void (*)(void))hook_entry_204, (void (*)(void))hook_entry_205, (void (*)(void))hook_entry_206, (void (*)(void))hook_entry_207, (void (*)(void))hook_entry_208, (void (*)(void))hook_entry_209, (void (*)(void))hook_entry_210, (void (*)(void))hook_entry_211, (void (*)(void))hook_entry_212, (void (*)(void))hook_entry_213, (void (*)(void))hook_entry_214, (void (*)(void))hook_entry_215, (void (*)(void))hook_entry_216, (void (*)(void))hook_entry_217, (void (*)(void))hook_entry_218, (void (*)(void))hook_entry_219, (void (*)(void))hook_entry_220, (void (*)(void))hook_entry_221, (void (*)(void))hook_entry_222, (void (*)(void))hook_entry_223, (void (*)(void))hook_entry_224, (void (*)(void))hook_entry_225, (void (*)(void))hook_entry_226, (void (*)(void))hook_entry_227, (void (*)(void))hook_entry_228, (void (*)(void))hook_entry_229, (void (*)(void))hook_entry_230, (void (*)(void))hook_entry_231, (void (*)(void))hook_entry_232, (void (*)(void))hook_entry_233, (void (*)(void))hook_entry_234, (void (*)(void))hook_entry_235, (void (*)(void))hook_entry_236, (void (*)(void))hook_entry_237, (void (*)(void))hook_entry_238, (void (*)(void))hook_entry_239, (void (*)(void))hook_entry_240, (void (*)(void))hook_entry_241, (void (*)(void))hook_entry_242, (void (*)(void))hook_entry_243, (void (*)(void))hook_entry_244, (void (*)(void))hook_entry_245, (void (*)(void))hook_entry_246, (void (*)(void))hook_entry_247, (void (*)(void))hook_entry_248, (void (*)(void))hook_entry_249, (void (*)(void))hook_entry_250, (void (*)(void))hook_entry_251, (void (*)(void))hook_entry_252, (void (*)(void))hook_entry_253, (void (*)(void))hook_entry_254, (void (*)(void))hook_entry_255 };
/* * NestedIntLib.h * * Created on: Dec 06, 2022 * Last Modified on: Dec 27, 2022 * Author: NoMaY * License: MIT */ #ifndef NESTEDINTLIB_H_ #define NESTEDINTLIB_H_ #define MY_BSP_CFG_UNNESTED_IPL_MAX 8 //Memo: //#define BSP_CFG_FIT_IPL_MAX (0xF) //#define configKERNEL_INTERRUPT_PRIORITY 1 //#define configMAX_SYSCALL_INTERRUPT_PRIORITY 4 #define INTERRUPT___0 PERMIT #define INTERRUPT___1 PERMIT #define INTERRUPT___2 PERMIT #define INTERRUPT___3 PERMIT #define INTERRUPT___4 PERMIT #define INTERRUPT___5 PERMIT #define INTERRUPT___6 PERMIT #define INTERRUPT___7 PERMIT #define INTERRUPT___8 PERMIT #define INTERRUPT___9 NOT_PERMIT // for debug purpos #define INTERRUPT__10 PERMIT #define INTERRUPT__11 PERMIT #define INTERRUPT__12 PERMIT #define INTERRUPT__13 PERMIT #define INTERRUPT__14 PERMIT #define INTERRUPT__15 PERMIT #define INTERRUPT__16 PERMIT #define INTERRUPT__17 PERMIT #define INTERRUPT__18 PERMIT #define INTERRUPT__19 PERMIT #define INTERRUPT__20 PERMIT #define INTERRUPT__21 PERMIT #define INTERRUPT__22 PERMIT #define INTERRUPT__23 PERMIT #define INTERRUPT__24 PERMIT #define INTERRUPT__25 PERMIT #define INTERRUPT__26 PERMIT #define INTERRUPT__27 PERMIT #define INTERRUPT__28 PERMIT #define INTERRUPT__29 PERMIT #define INTERRUPT__30 PERMIT #define INTERRUPT__31 PERMIT #define INTERRUPT__32 PERMIT #define INTERRUPT__33 PERMIT #define INTERRUPT__34 PERMIT #define INTERRUPT__35 PERMIT #define INTERRUPT__36 PERMIT #define INTERRUPT__37 PERMIT #define INTERRUPT__38 PERMIT #define INTERRUPT__39 PERMIT #define INTERRUPT__40 PERMIT #define INTERRUPT__41 PERMIT #define INTERRUPT__42 PERMIT #define INTERRUPT__43 PERMIT #define INTERRUPT__44 PERMIT #define INTERRUPT__45 PERMIT #define INTERRUPT__46 PERMIT #define INTERRUPT__47 PERMIT #define INTERRUPT__48 PERMIT #define INTERRUPT__49 PERMIT #define INTERRUPT__50 PERMIT #define INTERRUPT__51 PERMIT #define INTERRUPT__52 PERMIT #define INTERRUPT__53 PERMIT #define INTERRUPT__54 PERMIT #define INTERRUPT__55 PERMIT #define INTERRUPT__56 PERMIT #define INTERRUPT__57 PERMIT #define INTERRUPT__58 PERMIT #define INTERRUPT__59 PERMIT #define INTERRUPT__60 PERMIT #define INTERRUPT__61 PERMIT #define INTERRUPT__62 PERMIT #define INTERRUPT__63 PERMIT #define INTERRUPT__64 PERMIT #define INTERRUPT__65 PERMIT #define INTERRUPT__66 PERMIT #define INTERRUPT__67 PERMIT #define INTERRUPT__68 PERMIT #define INTERRUPT__69 PERMIT #define INTERRUPT__70 PERMIT #define INTERRUPT__71 PERMIT #define INTERRUPT__72 PERMIT #define INTERRUPT__73 PERMIT #define INTERRUPT__74 PERMIT #define INTERRUPT__75 PERMIT #define INTERRUPT__76 PERMIT #define INTERRUPT__77 PERMIT #define INTERRUPT__78 PERMIT #define INTERRUPT__79 PERMIT #define INTERRUPT__80 PERMIT #define INTERRUPT__81 PERMIT #define INTERRUPT__82 PERMIT #define INTERRUPT__83 PERMIT #define INTERRUPT__84 PERMIT #define INTERRUPT__85 PERMIT #define INTERRUPT__86 PERMIT #define INTERRUPT__87 PERMIT #define INTERRUPT__88 PERMIT #define INTERRUPT__89 PERMIT #define INTERRUPT__90 PERMIT #define INTERRUPT__91 PERMIT #define INTERRUPT__92 PERMIT #define INTERRUPT__93 PERMIT #define INTERRUPT__94 PERMIT #define INTERRUPT__95 PERMIT #define INTERRUPT__96 PERMIT #define INTERRUPT__97 PERMIT #define INTERRUPT__98 PERMIT #define INTERRUPT__99 PERMIT #define INTERRUPT_100 PERMIT #define INTERRUPT_101 PERMIT #define INTERRUPT_102 PERMIT #define INTERRUPT_103 PERMIT #define INTERRUPT_104 PERMIT #define INTERRUPT_105 PERMIT #define INTERRUPT_106 PERMIT #define INTERRUPT_107 PERMIT #define INTERRUPT_108 PERMIT #define INTERRUPT_109 PERMIT #define INTERRUPT_110 PERMIT #define INTERRUPT_111 PERMIT #define INTERRUPT_112 PERMIT #define INTERRUPT_113 PERMIT #define INTERRUPT_114 PERMIT #define INTERRUPT_115 PERMIT #define INTERRUPT_116 PERMIT #define INTERRUPT_117 PERMIT #define INTERRUPT_118 PERMIT #define INTERRUPT_119 PERMIT #define INTERRUPT_120 PERMIT #define INTERRUPT_121 PERMIT #define INTERRUPT_122 PERMIT #define INTERRUPT_123 PERMIT #define INTERRUPT_124 PERMIT #define INTERRUPT_125 PERMIT #define INTERRUPT_126 PERMIT #define INTERRUPT_127 PERMIT #define INTERRUPT_128 PERMIT #define INTERRUPT_129 PERMIT #define INTERRUPT_130 PERMIT #define INTERRUPT_131 PERMIT #define INTERRUPT_132 PERMIT #define INTERRUPT_133 PERMIT #define INTERRUPT_134 PERMIT #define INTERRUPT_135 PERMIT #define INTERRUPT_136 PERMIT #define INTERRUPT_137 PERMIT #define INTERRUPT_138 PERMIT #define INTERRUPT_139 PERMIT #define INTERRUPT_140 PERMIT #define INTERRUPT_141 PERMIT #define INTERRUPT_142 PERMIT #define INTERRUPT_143 PERMIT #define INTERRUPT_144 PERMIT #define INTERRUPT_145 PERMIT #define INTERRUPT_146 PERMIT #define INTERRUPT_147 PERMIT #define INTERRUPT_148 PERMIT #define INTERRUPT_149 PERMIT #define INTERRUPT_150 PERMIT #define INTERRUPT_151 PERMIT #define INTERRUPT_152 PERMIT #define INTERRUPT_153 PERMIT #define INTERRUPT_154 PERMIT #define INTERRUPT_155 PERMIT #define INTERRUPT_156 PERMIT #define INTERRUPT_157 PERMIT #define INTERRUPT_158 PERMIT #define INTERRUPT_159 PERMIT #define INTERRUPT_160 PERMIT #define INTERRUPT_161 PERMIT #define INTERRUPT_162 PERMIT #define INTERRUPT_163 PERMIT #define INTERRUPT_164 PERMIT #define INTERRUPT_165 PERMIT #define INTERRUPT_166 PERMIT #define INTERRUPT_167 PERMIT #define INTERRUPT_168 PERMIT #define INTERRUPT_169 PERMIT #define INTERRUPT_170 PERMIT #define INTERRUPT_171 PERMIT #define INTERRUPT_172 PERMIT #define INTERRUPT_173 PERMIT #define INTERRUPT_174 PERMIT #define INTERRUPT_175 PERMIT #define INTERRUPT_176 PERMIT #define INTERRUPT_177 PERMIT #define INTERRUPT_178 PERMIT #define INTERRUPT_179 PERMIT #define INTERRUPT_180 PERMIT #define INTERRUPT_181 PERMIT #define INTERRUPT_182 PERMIT #define INTERRUPT_183 PERMIT #define INTERRUPT_184 PERMIT #define INTERRUPT_185 PERMIT #define INTERRUPT_186 PERMIT #define INTERRUPT_187 PERMIT #define INTERRUPT_188 PERMIT #define INTERRUPT_189 PERMIT #define INTERRUPT_190 PERMIT #define INTERRUPT_191 PERMIT #define INTERRUPT_192 PERMIT #define INTERRUPT_193 PERMIT #define INTERRUPT_194 PERMIT #define INTERRUPT_195 PERMIT #define INTERRUPT_196 PERMIT #define INTERRUPT_197 PERMIT #define INTERRUPT_198 PERMIT #define INTERRUPT_199 PERMIT #define INTERRUPT_200 PERMIT #define INTERRUPT_201 PERMIT #define INTERRUPT_202 PERMIT #define INTERRUPT_203 PERMIT #define INTERRUPT_204 PERMIT #define INTERRUPT_205 PERMIT #define INTERRUPT_206 PERMIT #define INTERRUPT_207 PERMIT #define INTERRUPT_208 PERMIT #define INTERRUPT_209 PERMIT #define INTERRUPT_210 PERMIT #define INTERRUPT_211 PERMIT #define INTERRUPT_212 PERMIT #define INTERRUPT_213 PERMIT #define INTERRUPT_214 PERMIT #define INTERRUPT_215 PERMIT #define INTERRUPT_216 PERMIT #define INTERRUPT_217 PERMIT #define INTERRUPT_218 PERMIT #define INTERRUPT_219 PERMIT #define INTERRUPT_220 PERMIT #define INTERRUPT_221 PERMIT #define INTERRUPT_222 PERMIT #define INTERRUPT_223 PERMIT #define INTERRUPT_224 PERMIT #define INTERRUPT_225 PERMIT #define INTERRUPT_226 PERMIT #define INTERRUPT_227 PERMIT #define INTERRUPT_228 PERMIT #define INTERRUPT_229 PERMIT #define INTERRUPT_230 PERMIT #define INTERRUPT_231 PERMIT #define INTERRUPT_232 PERMIT #define INTERRUPT_233 PERMIT #define INTERRUPT_234 PERMIT #define INTERRUPT_235 PERMIT #define INTERRUPT_236 PERMIT #define INTERRUPT_237 PERMIT #define INTERRUPT_238 PERMIT #define INTERRUPT_239 PERMIT #define INTERRUPT_240 PERMIT #define INTERRUPT_241 PERMIT #define INTERRUPT_242 PERMIT #define INTERRUPT_243 PERMIT #define INTERRUPT_244 PERMIT #define INTERRUPT_245 PERMIT #define INTERRUPT_246 PERMIT #define INTERRUPT_247 PERMIT #define INTERRUPT_248 PERMIT #define INTERRUPT_249 PERMIT #define INTERRUPT_250 PERMIT #define INTERRUPT_251 PERMIT #define INTERRUPT_252 PERMIT #define INTERRUPT_253 PERMIT #define INTERRUPT_254 PERMIT #define INTERRUPT_255 PERMIT void NESTEDINTLIB_INT_HOOK_init(void); #endif /* NESTEDINTLIB_H_ */
#include "r_smc_entry.h" #include "NestedIntLib.h" void main(void); #define VECT_TRAP_1 1 #define VECT_TRAP_9 9 void main(void) { NESTEDINTLIB_INT_HOOK_init(); int_exception( VECT( TRAP, 9 ) ); set_ipl( MY_BSP_CFG_UNNESTED_IPL_MAX - 1 ); int_exception( VECT( TRAP, 1 ) ); set_ipl( MY_BSP_CFG_UNNESTED_IPL_MAX ); int_exception( VECT( TRAP, 1 ) ); set_ipl( MY_BSP_CFG_UNNESTED_IPL_MAX + 1 ); int_exception( VECT( TRAP, 1 ) ); for(;;); } uint32_t debug = 0x5a5a5a5a; #if defined(__CCRX__) /*----------------------------------------------------*/ #pragma inline_asm _acc_ static void _acc_(void){/* nothing is enough for `#pragma interrupt function_name(acc)` */} #pragma interrupt trap1_isr(vect = VECT(TRAP, 1), acc/* for debug purpose */) static void trap1_isr(void) { debug = 1; _acc_(); } #pragma interrupt trap9_isr(vect = VECT(TRAP, 9), acc/* for debug purpose */) static void trap9_isr(void) { debug = 9; _acc_(); } #elif defined(__GNUC__) /*--------------------------------------------------*/ static void trap1_isr(void) __attribute__ ((interrupt(R_BSP_SECNAME_INTVECTTBL, VECT(TRAP, 1)), used)); static void trap1_isr(void) { debug = 1; } static void trap9_isr(void) __attribute__ ((interrupt(R_BSP_SECNAME_INTVECTTBL, VECT(TRAP, 9)), used)); static void trap9_isr(void) { debug = 9; } #elif defined(__ICCRX__) /*-------------------------------------------------*/ #pragma vector = VECT(TRAP, 1) static __interrupt void trap1_isr(void) { debug = 1; } #pragma vector = VECT(TRAP, 9) static __interrupt void trap9_isr(void) { debug = 9; } #endif /*-------------------------------------------------------------------*/