こんにちは。NoMaYです。ひとつ立ててみました。[関連リンク]以下、大昔の話題ですけれども。RX65NのSCIgのTENDフラグの挙動を調べてみた(RX631のSCIcのTENDフラグの挙動も調べてみた)community-ja.renesas.com/cafe_rene/forums-groups/mcu-mpu/rx/f/forum5/5642/rx65n-scig-tend-rx631-scic-tend
こんにちは。NoMaYです。以下のスレッドに関わって気になったのですけれども、電圧監視0リセットの解除電圧に関して、電源投入時の挙動がドキュメントの記載から素朴に予想される挙動と実際の挙動とで異なっているようです。RX130とRX231に関して以下のスレッドにて投稿がありました。パワーオンリセットと電圧監視0リセットの関係についてcommunity-ja.renesas.com/cafe_rene/forums-groups/mcu-mpu/rx/f/forum5/6294/threadRx231の起動時リセットについてcommunity-ja.renesas.com/cafe_rene/forums-groups/mcu-mpu/rx/f/forum5/10390/rx231