Da14531 codeless安全配对模式

我通过设置sec_pair_mode来改变安全配对模式,可以实现连接时需要PIN密码进行配对连接,但是每次codeless设备重新上电都需要输入密码配对,有没有方法在不改密码的情况下只配对一次?

Parents Reply
  • Hi Mund,

    DA14531MOD 的flash 是1MB的。

    1,如果你需要OTA功能,参考这里的例程,用户数据可以存储在 Product Header后面。

    SUOTA APP - DA14531 ota development - Bluetooth Low Energy - Wireless Connectivity - Renesas Engineering Community

    2,如果不需要OTA功能,数据可以存在最后一个4K sector 0x1F000-0x20000, 如果4K不够可以继续向上申请。并且适当调整 默认绑定信息的存储位置。

    BR,

    JH_Renesas

Children
No Data